Power & Energy
  • Technologies
  • More
Power & Energy
Forum calcolo dissipazione
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 283 subscribers
  • Views 1484 views
  • Users 0 members are here
  • dissipazione
Related

calcolo dissipazione

e14 Contributor
e14 Contributor over 16 years ago

Salve a tutti,

sapreste indicarmi un software online o free per il calcolo della resistenza termica di semplici dissipatori (es barre di alluminio)?

Grazie a tutti

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Something like http://www.novelconceptsinc.com/calculators-cylinder-thermal-resistance.cgi ?

    (or possibly something else from http://www.novelconceptsinc.com/calculators.htm?)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor

    Dear friend,

    the link that you gave me is a web page that I know well, but I think that calculation of that program is completely wrong! For example from link  http://www.novelconceptsinc.com/calculators.htm if you choose the chapter "Slab Thermal Resistance", with an alluminia dissipator (thermal conductivity 236 W/mK), with dimensions 360mmX200mmX4mm) the result is a thermal resistance of 2.35405e-04 C/W!

    It' s absolutely impossible that the thermal resistance of this structure is so low

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor

    Using R=I/k and Windows Calculator:


    R = 0.004/236 = 1.6949152542372881355932203389831e-5  (4mm / 236w/m.K)

     

    R/(0.36*0.2) = 0.0002354048964218455743879472693032   approximately  2.354x10^-4

     

    (Both the website and myself may be wrong, though.  Maths is not one of my stronger subjects!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lpetacchi
    0 lpetacchi over 15 years ago in reply to e14 Contributor

    Your calculation is correct. Thermal resistance in this case is between two planes of the object. "Dissipazione" refers to the capability to transfer heat (heat sinking) to the ambient, mainly by convection; this number is usually quite higher.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Senza tante complicazioni io uso un metodo approssimativo ma efficace per superfici fino a circa 10x10 cm (200 cm²):

    Rt = 1 / S x K

    dove Rt = resistenza termica del dissipatore, in °C/W

    S = superficie (totale, quindi entrambi i lati) della lamiera, in cm²

    K = 0.003 per alluminio 3 mm superficie anodizzata; 0.0025 alluminio 3 mm naturale; 0.002 alluminio 2 mm naturale;

    Se il dissipatore è un profilato alettato K = 0.0075 in aria ferma, K = 0.015 con flusso d'aria di 25 l/min

    es. dissipatore piano 5x5 cm sp 3mm in aria ferma: S=50 cm², K= 0.0025, Rt = 8 °C/W