Power & Energy
  • Technologies
  • More
Power & Energy
Forum Linear or Switch Mode Power supply for PWM Driven Stepper Motors?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 284 subscribers
  • Views 5973 views
  • Users 0 members are here
  • management
  • stepper_motor
  • power_management
  • power_distribution
  • power_supply
  • power
Related

Linear or Switch Mode Power supply for PWM Driven Stepper Motors?

Catwell
Catwell over 16 years ago

I used to use linear power supplies for all my motor control applications. Stepper and servo drivers were all fed with raw linear power. However, recently I have switched to less expensive switching power supplies for the same application. Although I have not seen any performance drop in the motors, I am wondering if I should still stick with a linear supply.


So, to all the motor drive designers out there, is there any real problems with using a switching supply? Would I get smoother motor commutation going linear?


For those who want to know, I am driving 2.1 - 3A per phase stepper motors at 36V. The power supply I am now using supplies switch mode regulated power of 36V at up to 8.8A (350W).


Cabe

  • Sign in to reply
  • Cancel
Parents
  • enrico.migchels
    0 enrico.migchels over 16 years ago

    Hi Cabe,

     

    Your qoute: "The power supply I am now using supplies switch mode regulated power of 36V at up to 8.8A (350W)"

     

    Similar product 8A/40Vdc and 8A/5Vdc (main converter), 1A/5Vdc (separate standby converter), Triac controlled (PIC16F648A) AC induction motor (900W) .

    Dimensions L: 190mm, W: 90mm H: 50mm

     

    image

    As this power supply has a DC-power stage of more than 350W, i'm wondering what the dimensions are from your power supply. I build this power supply for a robot vacuum cleaner with AC induction motor (suction) and several Brushless-DC-motors (drive, cordwinder). Maybe i have to add that the AC input is 230Vac and that there is a fan cooling the device.

     

    Best regards,

     

    Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • enrico.migchels
    0 enrico.migchels over 16 years ago

    Hi Cabe,

     

    Your qoute: "The power supply I am now using supplies switch mode regulated power of 36V at up to 8.8A (350W)"

     

    Similar product 8A/40Vdc and 8A/5Vdc (main converter), 1A/5Vdc (separate standby converter), Triac controlled (PIC16F648A) AC induction motor (900W) .

    Dimensions L: 190mm, W: 90mm H: 50mm

     

    image

    As this power supply has a DC-power stage of more than 350W, i'm wondering what the dimensions are from your power supply. I build this power supply for a robot vacuum cleaner with AC induction motor (suction) and several Brushless-DC-motors (drive, cordwinder). Maybe i have to add that the AC input is 230Vac and that there is a fan cooling the device.

     

    Best regards,

     

    Enrico Migchels