Power & Energy
  • Technologies
  • More
Power & Energy
Forum Boost 5V (4.7v) to 9V
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 285 subscribers
  • Views 5248 views
  • Users 0 members are here
  • 9v
  • 5vdc
Related

Boost 5V (4.7v) to 9V

tim687
tim687 over 10 years ago

I've got a 5V (4.7v) powerbank, and I need 9V to run my Arduino and the dc motors.

 

I couldn't find any circuit online.

 

Can somebody help me?

 

 

Thanks in advance,

 

Tim

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 10 years ago +1
    Hi Tim, How about a boost converter like this? http://www.ebay.com/itm/DC-DC-2A-Adjustable-Boost-Power-Supply-Converter-Step-Up-Module-2-24v-Input-New-/161650445447?hash=item25a31e0c87 John Cheaper to…
  • mcb1
    mcb1 over 10 years ago +1
    Tim John is quite right. There is one thing to consider though. You haven't specified what the ratings are for the 9v motors. All motors will tend to draw twice the running current when starting, and this…
Parents
  • tim687
    tim687 over 10 years ago

    Thanks for your answers!

     

    The motors don't run from the 5V connection from the Arduino ;-)

     

    But no capacitor is there for the motors. I'll try to add them.

     

    Btw, the motors sort of run at 5V, but I might still be buying the step up module soon!

     

    Thanks!

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to tim687

    It is probably not a good idea to run the motors from the Arduino 5 volt power. Motors usually take more current than the Arduino  can supply. Also it will be a good idea to put a diode across the motor to protect the rest of your circuit from Inductive spikes. Check out "Flyback Diode or Freewheeling Diode". The Capacitor that Mark recommended will not help the motor run but it will help prevent the motor from resetting the Arduino. Your best approach is to use the Arduino to control a MOSFET or a Transistor and use the Transistor to control a higher voltage that is being used to drive the motors.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 10 years ago in reply to tim687

    It is probably not a good idea to run the motors from the Arduino 5 volt power. Motors usually take more current than the Arduino  can supply. Also it will be a good idea to put a diode across the motor to protect the rest of your circuit from Inductive spikes. Check out "Flyback Diode or Freewheeling Diode". The Capacitor that Mark recommended will not help the motor run but it will help prevent the motor from resetting the Arduino. Your best approach is to use the Arduino to control a MOSFET or a Transistor and use the Transistor to control a higher voltage that is being used to drive the motors.

    John