Power & Energy
  • Technologies
  • More
Power & Energy
Forum variable power supply using National Semiconductor LM22679-ADJ ?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 284 subscribers
  • Views 377 views
  • Users 0 members are here
  • switchmode
  • lm22679
Related

variable power supply using National Semiconductor LM22679-ADJ ?

Former Member
Former Member over 15 years ago

Will it be possible to design a variable power supply using National Semiconductor LM22679-ADJ ??

 

  Input 32 Volt DC

  Out :  10 to 30 Volt DC using potentiometer

  Current  :  Max.  5A

 

Who has some experience to share ??

##

  • Sign in to reply
  • Cancel
  • lpetacchi
    0 lpetacchi over 15 years ago

    Hi,

    LM22679 has a maximum duty cycle <90%; with 32V at the input the maximum output voltage @5A could be 27..28V.

    Using an LM22677 at 200kHz the target is achievable, but with the use of high performance inductor and diode.

    Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 15 years ago in reply to lpetacchi

       I want to be able to adjust the LM22679 -adj output voltage with a trim potentiometer from 10 to 30v .

    .. Any suggestions for the optimal values for the components .

    .. I have tryed the National Semiconductor Web-Bench simulation tool , but only fixed values and fixed voltages are possible in

      this simulation tool -   And I have tryed to contact National Semiconductor , but gets no answer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer