Power & Energy
  • Technologies
  • More
Power & Energy
Forum DC-DC 5W-15W, 12V to 300V-1.2kV
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 283 subscribers
  • Views 1285 views
  • Users 0 members are here
Related

DC-DC 5W-15W, 12V to 300V-1.2kV

e14 Contributor
e14 Contributor over 15 years ago

DC-DC 5W-15W, 12V to 300V-1.2kV

 

1. Can I use current sense transformer for step-up to kV?

2. Where to buy step-up to HV transformer for specified power range?

3. That power IC recommeded for this application? Voltage adjustability is nessecary, trimmer is OK.

4. Is it possible to step-up from 12V to kV with non transformed based topology?

 

Thanks,

John

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Current sense transformer - unlikely because the insulation rating on the winding is not intended for anything other than a few tens of volts maximum. However, you might be lucky and get 100V. Frequency of operation is something to consider - if you want a fairly smooth DC output (i.e. small ripple under load) then operating at power AC frequencies is probably not a good idea (although many years ago X-ray machines did use exactly such a technique). These days 50kHz is somewhere about right for switch-mode step up converters but they do tend to use ferrite transformers to achieve this - look at linear technologies website - they have designs that can certainly provide enough voltage for electroluminescent displays (300V ish). Four of these building blocks could have their outputs wired in series. Another thing to remember about these sorts of designs is that the transformer provides much needed isolation and protection both to the primary circuit and the user/operator. Televisions use a transformer to get several kV AC then a diode tripler to get (say) 25kV needed for the tube. I've seen designs (on x-ray machines) that used 7 stages of diode capacitor to boost the voltage but directly from 12V to 1kV would need far too many and I suspect the losses would be too great.

     

    Alternatively I bet you could buy one - what budget do you have? How many units? what ripple on the output? Do you need feedback control to keep the output regulated.

     

    Sorry for the long answer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    I expect to build for 5-15Eur for components and assembly. Without feedback for the same power is possible to get for 3-5Eur. I can't find step-up transformers for photo flash lamps. They might be suitable for me.

    Usage 100-1000units per year. Load is not fixed, so feedback is nessecary. Ripples 2% and long therm stability is OK.

    I made experiment with current sense transformer. With 3V spike, I get ~300V in the output.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Try searching for a pdf of an LT3573EMSE#PBFLT3573EMSE#PBF from linear technology - they have a circuit for a 300V isolated output (page 23). Four circuits would work with the outputs wired in series - if you contact LT they may even recommend a transformer that goes straight up to 1.2kV - this would be better because you'd get better control BUT you may not get enough power. They will advise - they are pretty good at helping but don't expect answers as quick as this one!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Thanks for fast answer! So far biggest problem to find commercialy available right transformer. I see right transformers in various devices, but googling for part number doesn't work.

     

    Jonas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    Jonas,  You could try to use a CCFL-inverter. A CCFL-inverter is a high voltage generator for LCD background lighting, scanners etc. A single CCFL lamp usually needs 1000 Volt and 5 mA. The current is limited by a series capacitor. They are  available at prizes below $8 at several suppliers. You could only use the high voltage transformer from the CCFL-inverter and make your own driver circuit with feedback.  Johan.