Power & Energy
  • Technologies
  • More
Power & Energy
Forum DC-DC 5W-15W, 12V to 300V-1.2kV
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 283 subscribers
  • Views 1306 views
  • Users 0 members are here
Related

DC-DC 5W-15W, 12V to 300V-1.2kV

e14 Contributor
e14 Contributor over 15 years ago

DC-DC 5W-15W, 12V to 300V-1.2kV

 

1. Can I use current sense transformer for step-up to kV?

2. Where to buy step-up to HV transformer for specified power range?

3. That power IC recommeded for this application? Voltage adjustability is nessecary, trimmer is OK.

4. Is it possible to step-up from 12V to kV with non transformed based topology?

 

Thanks,

John

  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    Jonas,  You could try to use a CCFL-inverter. A CCFL-inverter is a high voltage generator for LCD background lighting, scanners etc. A single CCFL lamp usually needs 1000 Volt and 5 mA. The current is limited by a series capacitor. They are  available at prizes below $8 at several suppliers. You could only use the high voltage transformer from the CCFL-inverter and make your own driver circuit with feedback.  Johan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    Jonas,  You could try to use a CCFL-inverter. A CCFL-inverter is a high voltage generator for LCD background lighting, scanners etc. A single CCFL lamp usually needs 1000 Volt and 5 mA. The current is limited by a series capacitor. They are  available at prizes below $8 at several suppliers. You could only use the high voltage transformer from the CCFL-inverter and make your own driver circuit with feedback.  Johan.