Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging two GP Ion-Li Battery packs with only one IC?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 4 answers
  • Subscribers 282 subscribers
  • Views 4989 views
  • Users 0 members are here
  • pack
  • li-ion
  • battery
  • charger
Related

Charging two GP Ion-Li Battery packs with only one IC?

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

I have this two Li-Ion Battery packs from GP Batteries:

 

7.4V

http://es.farnell.com/jsp/search/productdetail.jsp?SKU=1848661

 

11.1V

http://es.farnell.com/jsp/search/productdetail.jsp?SKU=1848662

 

I have put them in series -> 18.5V

I want them to charge with for example LTC4008EGN#PBFLTC4008EGN#PBF from Linear Tech.

http://es.farnell.com/linear-technology/ltc4008egn-pbf/cargador-de-baterias-smd-ssop20/dp/1273983?Ntt=ltc4008

 

Question is, what happens if one of the packs is medium-charged and the other completely discharged? I understand that in a certain moment one of the packs will be charged, but what happens with the other pack?

Will continue charging? Will the charged pack be damaged? Or simply one of the packs will remain without being charged?

 

Is it imperative in this scenario to use one charger for each pack??

 

Thanks for any tip.

 

Regards,

 

Cristian.


  • Sign in to reply
  • Cancel
Parents
  • RWM
    0 RWM over 14 years ago

    Hi Cristian,

     

    as battery packs are equipped with protection circuits (over-charge over-discharge etc. - see datasheet page 6), they should be charged separately. If two packs will be connected in series and will be in different state of charge, when charging protection circuit in one pack will detect overvoltage, it will disconnect this pack, so charging of second pack will be stopped.

     

    If there will be other battery pack without protection circuits, it would be possible to connect packs in series and charge from one charger but blancing circuit should be used. It protects cells from overcharging.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    Thank you for your answer RWM,

    I was thinking about that... as I fear.

     

    From the two packs I received, only one of them has a third white terminal (cable). Is this a voltage related to the temperature? Can I connect this cable directly to the Thermistor Voltage In (of the IC charger)?

    The other pack has only two terminals... so, I don´t know, maybe buy a thermistor and put it inside the second pack? So each IC charger receives the temperature of their associated pack. Is this a normal way you think?

     

    Best Regards,

     

    Cristian.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    Thank you for your answer RWM,

    I was thinking about that... as I fear.

     

    From the two packs I received, only one of them has a third white terminal (cable). Is this a voltage related to the temperature? Can I connect this cable directly to the Thermistor Voltage In (of the IC charger)?

    The other pack has only two terminals... so, I don´t know, maybe buy a thermistor and put it inside the second pack? So each IC charger receives the temperature of their associated pack. Is this a normal way you think?

     

    Best Regards,

     

    Cristian.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    Interesting, according to product pages on farnell.com and datasheets both modules should have three wires, you have got different model? Anyway, I have not found wires description neither in datasheet nor on gpbatteries web site. I can guess that there is connected 10kohm thermistor between V- and white wire, but you should check this using ohmmeter. If this is not true, you can attach themistor to the pack. It is not necessary to put it inside the pack, it can be attached on outside sleeve but on battery cell (glued for example). Same for second pack. Themistor can be connected to charger NTC input as in datasheet. It is used to determine whether battery temperature is in safe area for charging (usually 0-40 deg C).

     

    I do hope this will help.

     

    Best regards,

     

    Ryszard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    Well, about the third terminal it happened with the 14.8V model (with only two terminals)... but anyway it´s more clear now.

    This has helped a lot.

     

    Regards,

     

    Cristian