Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging two GP Ion-Li Battery packs with only one IC?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 4 answers
  • Subscribers 282 subscribers
  • Views 4989 views
  • Users 0 members are here
  • pack
  • li-ion
  • battery
  • charger
Related

Charging two GP Ion-Li Battery packs with only one IC?

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

I have this two Li-Ion Battery packs from GP Batteries:

 

7.4V

http://es.farnell.com/jsp/search/productdetail.jsp?SKU=1848661

 

11.1V

http://es.farnell.com/jsp/search/productdetail.jsp?SKU=1848662

 

I have put them in series -> 18.5V

I want them to charge with for example LTC4008EGN#PBFLTC4008EGN#PBF from Linear Tech.

http://es.farnell.com/linear-technology/ltc4008egn-pbf/cargador-de-baterias-smd-ssop20/dp/1273983?Ntt=ltc4008

 

Question is, what happens if one of the packs is medium-charged and the other completely discharged? I understand that in a certain moment one of the packs will be charged, but what happens with the other pack?

Will continue charging? Will the charged pack be damaged? Or simply one of the packs will remain without being charged?

 

Is it imperative in this scenario to use one charger for each pack??

 

Thanks for any tip.

 

Regards,

 

Cristian.


  • Sign in to reply
  • Cancel
Parents
  • shoker4
    0 shoker4 over 14 years ago

    Hi Christian, by the characteristics of the battery I guess the use to R / C, told him that I had the same problem with Li-Ion batteries are quite sensitive with respect to the overtemperature and overvoltage. In addition, the battery pack that I use are of high capacity (5000mAh) and Vienne linked in series-parallel with no internal protection. I decided to break the pack and reset CI placed a pair of of protection against overload / over temperature and also balances the load of the cell. For the latter decided to take a pair of wires to each cell to the back of the pack and charger by using a load cell by cell in a battery, a load at the end of the cables so that the pack is reinforced parallel series. As an additional point of C.I. also use the download intelligently manage each cell preventing its voltage falls below 3.3V, which were to happen if the cell loses its ability to recharge.

     

     

     

    Then I leave the link in the catalog in which the CI search more suitable to my application.

     

    http://www.ti.com/lit/sg/slyt420/slyt420.pdf

     

    Att. Gustavo (sorry my english is bad)

     

     

    This is the original pack modifying:

    image

     

     

     

    __________________________________________________________________________________________________________________________________________

     

     

    Hola cristian, por las caracteristicas de la bateria me imagino que la utilizarás para R/C, le comento que yo tuve el mismo inconveniente con las baterias Li-Ion, son bastante delicadas con respecto a la sobretemperatura y sobrevoltaje. Además los pack de bateria que utilizo son de alta capacidad (5000mah) y vienne unidas en serie-paralelo sin ninguna proteccion interna. Decidi deshacer el pack y rearmarlo colocandole un par de C.I. de proteccion contra sobrecarga/sobretemperatura y además balancea la carga de la celda. Para esto ultimo decidi sacar un par de cables a cada celda hacia el lado posterior del pack y utilizando un cargador mediante cargar celda por celda en un cargador, al finalizar la carga uno los cables de tal manera que queda armado el pack serie paralelo. Como punto adicional los C.I. que utilice tambien gestionan inteligentemente la descarga de cada celda evitando que su tensión descienda por debajo de 3.3v, que si llegara a pasar la celda pierde su capacidad de recargarse.

     

    A continuación le dejo el link del catalogo en el cual busque los C.I. mas adecuados a mi aplicacion.

     

    http://www.ti.com/lit/sg/slyt420/slyt420.pdf

     

    Atte. Gustavo

     

    Este es el pack original que modifique:

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shoker4
    0 shoker4 over 14 years ago

    Hi Christian, by the characteristics of the battery I guess the use to R / C, told him that I had the same problem with Li-Ion batteries are quite sensitive with respect to the overtemperature and overvoltage. In addition, the battery pack that I use are of high capacity (5000mAh) and Vienne linked in series-parallel with no internal protection. I decided to break the pack and reset CI placed a pair of of protection against overload / over temperature and also balances the load of the cell. For the latter decided to take a pair of wires to each cell to the back of the pack and charger by using a load cell by cell in a battery, a load at the end of the cables so that the pack is reinforced parallel series. As an additional point of C.I. also use the download intelligently manage each cell preventing its voltage falls below 3.3V, which were to happen if the cell loses its ability to recharge.

     

     

     

    Then I leave the link in the catalog in which the CI search more suitable to my application.

     

    http://www.ti.com/lit/sg/slyt420/slyt420.pdf

     

    Att. Gustavo (sorry my english is bad)

     

     

    This is the original pack modifying:

    image

     

     

     

    __________________________________________________________________________________________________________________________________________

     

     

    Hola cristian, por las caracteristicas de la bateria me imagino que la utilizarás para R/C, le comento que yo tuve el mismo inconveniente con las baterias Li-Ion, son bastante delicadas con respecto a la sobretemperatura y sobrevoltaje. Además los pack de bateria que utilizo son de alta capacidad (5000mah) y vienne unidas en serie-paralelo sin ninguna proteccion interna. Decidi deshacer el pack y rearmarlo colocandole un par de C.I. de proteccion contra sobrecarga/sobretemperatura y además balancea la carga de la celda. Para esto ultimo decidi sacar un par de cables a cada celda hacia el lado posterior del pack y utilizando un cargador mediante cargar celda por celda en un cargador, al finalizar la carga uno los cables de tal manera que queda armado el pack serie paralelo. Como punto adicional los C.I. que utilice tambien gestionan inteligentemente la descarga de cada celda evitando que su tensión descienda por debajo de 3.3v, que si llegara a pasar la celda pierde su capacidad de recargarse.

     

    A continuación le dejo el link del catalogo en el cual busque los C.I. mas adecuados a mi aplicacion.

     

    http://www.ti.com/lit/sg/slyt420/slyt420.pdf

     

    Atte. Gustavo

     

    Este es el pack original que modifique:

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to shoker4

    Hi Gustavo,

     

    I´ve also looked for this type of batteries. But I think that packs which are sold in the market that includes protection circuit are also included with a balance charge circuit. The only problem is that they don´t have temperature protection, some of them without even thermistor. (correct me if I´m wrong)

     

    According to the post with RWM, I´ve been speaking with tenergy about prices of pack batteries with temperature protection included (5 cells - 4,400mAH) but prices goes too high. So the best solution I have is to implement temperature protection by myself, (IC or whatever.).

     

    The link of Texas Instruments pdf shows nice ICs for implementation. But I don´t see the difference buying one pack with protection included (5 cells in a pack) than buying a battery without any electronic inside the pack.

     

    Regards,

     

    Cris