Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging two GP Ion-Li Battery packs with only one IC?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 4 answers
  • Subscribers 282 subscribers
  • Views 5003 views
  • Users 0 members are here
  • pack
  • li-ion
  • battery
  • charger
Related

Charging two GP Ion-Li Battery packs with only one IC?

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

I have this two Li-Ion Battery packs from GP Batteries:

 

7.4V

http://es.farnell.com/jsp/search/productdetail.jsp?SKU=1848661

 

11.1V

http://es.farnell.com/jsp/search/productdetail.jsp?SKU=1848662

 

I have put them in series -> 18.5V

I want them to charge with for example LTC4008EGN#PBFLTC4008EGN#PBF from Linear Tech.

http://es.farnell.com/linear-technology/ltc4008egn-pbf/cargador-de-baterias-smd-ssop20/dp/1273983?Ntt=ltc4008

 

Question is, what happens if one of the packs is medium-charged and the other completely discharged? I understand that in a certain moment one of the packs will be charged, but what happens with the other pack?

Will continue charging? Will the charged pack be damaged? Or simply one of the packs will remain without being charged?

 

Is it imperative in this scenario to use one charger for each pack??

 

Thanks for any tip.

 

Regards,

 

Cristian.


  • Sign in to reply
  • Cancel
Parents
  • RWM
    0 RWM over 14 years ago

    Hi Cristian,

     

    as battery packs are equipped with protection circuits (over-charge over-discharge etc. - see datasheet page 6), they should be charged separately. If two packs will be connected in series and will be in different state of charge, when charging protection circuit in one pack will detect overvoltage, it will disconnect this pack, so charging of second pack will be stopped.

     

    If there will be other battery pack without protection circuits, it would be possible to connect packs in series and charge from one charger but blancing circuit should be used. It protects cells from overcharging.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    Hi,

     

    I have chosen two IC Chargers for each of the two Li-Ion packs. Now when I´m going to design the circuit I realize that if this two packs are connected in series, the GND of the 24V that powers the two IC chargers must be different on each other.

     

    It´s an automatic charger so I can´t disconnect the packs. So, do I need two source powers? I fear that it will be the only possibility... Anyone has pass through this?

     

    Thanks in advance

     

    Regards,

     

    Cristian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    Hi,

     

    as these packs have protection circuits which can disconnect pack, you have some options:

    1) use 2 floating power sources (it means GND of both sources not connected, as GND will be connected to negative electrode of power pack),

    2) remove protection circuits from power packs, connect them in series and use one charger; however, you should add protection circuit for 5 cells (for example http://www.ti.com/product/bq77pl157a4225 or more advanced

    http://es.farnell.com/texas-instruments/bq77pl900dl/ic-battery-protec-li-ion-10cell/dp/1640400).

     

    Regards,

     

    Ryszard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    Thanks for the links Ryszard,

     

    I´m considering also buying a 5-cell pack. Is not very usual. But I saw that some companies like "Tenergy" sells chargers and packs of more than 4 cells. Well, packs of 5 cell does not appear in the web, but I think that is probably easy to find this.

    Then, the charger could be a LTC008 for example, with adjustable output voltage, so a termination charger IC could be use for specific Ion-Li charge. This termination charger IC should be connected to the LTC008 or similar...

     

    But I can´t understand because here:

    http://www.all-battery.com/AT_TenergyLi-Ion18.5V2600mAhRechargeablePackwithPCB-31941.aspx

    we see a 5-cell pack from tenergy.

     

    But in the official web site:

    http://www.tenergy.com/Site/Li-Ion-Category

    It does not appear...

     

    All depends on the difficulty of finding a 5-cell Li-Ion pack... Do you have any recommendation for finding it?

    Tenergy company seems not to answer for the request email I sended...

     

    All the best,

     

    Cristian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    Hi Cristian,

     

    you have some packs there:

    http://www.batteryspace.com/Ultra-High-Energy-Li-Ion-18650-Battery-18.5V-2800mAh-51.8Wh-4.2A-rate.aspx

    http://www.batteryspace.com/Li-Ion-18650-Battery-18.5V-2600mAh-48.1Wh-7.0A-rate-Battery-Pack.aspx

     

    If battery pack is available at all-batterycom and not at tenergy.com so perhaps it is intended for OEM customers. If datasheet is available, it can be used.

     

    I don't know LTC008, you can use e.g. LTC4008EGN#PBFLTC4008EGN#PBF, MAX17015B

     

    Best regards,

     

    Ryszard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    Hi again,

     

    After researching, I´ve decided to implement a 5-cell charger with 5-cell pack.

    Problem is that there is no specific Li-Ion charger LTC family for 5-cells.

    LTC4007 is Li-Ion Specific charger up to 4cells

    LTC4008 is standard charger with regulated output voltage up to 28V

     

    I´m not sure of what elements are needed for making a specific Li-Ion / Li-Po charger with LTC4008. I know that there is some chips for making the charger specific for certain chemistry...

     

    Best Regards,

     

    Cristian.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    Hi,

     

    LTC4008 is intended for various Lithium cells so you don't need aditional chips. All you need is to calculate some components based on datasheet http://cds.linear.com/docs/Datasheet/4008fb.pdf and that is all.

     

    Firstly you should determine charging current. Maximum current depends on cell model, capacity and manufacturer - best to find in pack datasheet. Usually it is in 0.8-1C range (where C - current value equal to capacity value, e.g. if you have 2000mAh pack, it will be 2000mA). Of couse there is also power supply which can limit charging current too.

     

    Secondly you should calculate float voltage (end of charge voltage). For most Li-Ion cels it is 4.2V, so you should set in to 5*4.2V=21.0V.

     

    Then you can calculate component values (from page 13 in datasheet).

     

    Best regards,

     

    Ryszard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    Hi Ryszard,

     

    Thanks for the answer, I would like to remake the question again.

    LTC4008 says:

    LTC4008 - 4A, High Efficiency, Multi-Chemistry Battery Charger

    -General Purpose Charger Controller

     

    LTC4007:

    LTC4007 - 4A, High Efficiency, Standalone Li-Ion Battery Charger

    Complete Charger Controller for 3- or 4-Cell Lithium-Ion Batteries

    Built-In Charge Termination for Li-Ion Batteries

     

    So question is: what is "Li-ion charge termination"?

     

    I don´t believe LTC4008 is for use "only" with Li-ion

     

    This question is around my head during last 2 months image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    Hi Cristian,

     

    LTC4008 is constant current/constant voltage charger. This method is used mainly to charge various Lithium cells (Li-Ion, Li-Poly, LiFePO4) but can also be used to charge lead-acid batteries. For other chemistries is not recommended (NiCd and NiMH use mainly -dV method), but if you set float voltage as safety limit and add -dV detection, you can charge also Ni-based batteries.

     

    Termination of Li-Ion charging is when charging current decline to 0.05-0.3 of current in constant current mode. LTC4008 has FLAG output which is set low when charging current fall to C/10, so it can be used to e.g. shutdown charge using SHDN input. You can also connect FLAG to microcontroller which will shutdown charger usign SHDN input and also will monitor FAULT flag but this is not necessary.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    I found a document in Linear Tech, "Next Generation No Compromise

    Battery Chargers" that explains more deeply this concept.

    Yes, it can be charged without these features but there is 1 point that could be missed:

     

    - Low Battery Conditioning

     

    If batteries are totally discharged, LTC4006 and LTC4007 charge the battery slowly until it reaches tipical voltage to start a normal charge (faster), this maybe prolongs battery life.. a pity.. jeje, I think I will take

     

    Well, I think it´s clear now and I´m driving the topic outside of its range. image

    I will use LTC4008, thanks for the tips!

     

    All the Best,

     

    Cristian.

     

     

     

     

     

     

     

    Next Generation No Compromise
    Battery Chargers
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    I found a document in Linear Tech, "Next Generation No Compromise

    Battery Chargers" that explains more deeply this concept.

    Yes, it can be charged without these features but there is 1 point that could be missed:

     

    - Low Battery Conditioning

     

    If batteries are totally discharged, LTC4006 and LTC4007 charge the battery slowly until it reaches tipical voltage to start a normal charge (faster), this maybe prolongs battery life.. a pity.. jeje, I think I will take

     

    Well, I think it´s clear now and I´m driving the topic outside of its range. image

    I will use LTC4008, thanks for the tips!

     

    All the Best,

     

    Cristian.

     

     

     

     

     

     

     

    Next Generation No Compromise
    Battery Chargers
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    Interesting document.

     

    Sometimes charging of deeply discharged battery can damage it, so it is better to implement low battery conditioning. Schematic is on figure 6 on page 14 in LTC4008 datasheet. You can drive Q1 using comparator/op-amp (when battery voltage is lower than 15V->3.0V/cell) or microcontroller if you will use it.

     

    I do hope your charger will work good.

     

    Best regards,

     

    Ryszard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    image Good point. and very easy implementation.

     

    Ahh I hope so too, the only thing that scares me a bit is the mosfet´s gates. I remember that once in a project of an industrial printer, in the power section with Step-Down Converters, we spent a couple of months trying to know why the mosfets break down when plugging the system. I spent one month totally confused, I remember it like a nightmare, later another engineer and the same... the problem was resolved changing the CC/CC chip... don´t remember the brand... I only remember my desk full of mosfets and dreaming with some fantastic sculpture with all those broken mosfets, jajaj.

     

    I hope LTC4008 to be polite with the mosfets. I´ll try to post the results.

     

    Cheers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    If you will keep tracks from IC to transistor gate short, I think there should not be any problems. As gate drive voltage is 5.6V typically, you should use logic-level MOSFETs.

     

    I wish you success with your design.

     

    All the best!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    Response from LTC factory applications

     

    Cristian, it seems as if your questions have already been answered, but we’d still like to make some comments. In general, the greater number of batteries in series and greater capacity would require charge balancing. 3-4 series cells and up tends to be a general manufacturer borderline for cell balancing.  Farnell should be able to comment on this. Tenergy would likely say the same. And by the way, Tenergy does make 5-cell packs and can make one-off packs of pretty much any number of series cells. I’m not sure if your application is a low-volume consumer, private hobbyist, etc. Could you advise? We should be able to either suggest a pack for your usage (if you haven’t already chosen one) or get you in touch with the sales guys that could help you develop a one-off 5-cell pack. We have asked for this in the past for reference designs.
     
    As you’ve already considered, if charging two distinct packs of 2 and 3-cells respectively, one could get away with two separate chargers without balancing. Since the batteries are stacked, you & Ryszard have correctly observed that the “top” charger for the upper cells of the stack would need to float in series from the “bottom” charger. You could reference that circuit’s GND from the VBAT+ of the lower circuit, but you would still need an isolated connection to the input side of each charger. It would be necessary to have a front-end isolated topology, such as a dual output winding flyback to take the wall adapter input. This would actually be helpful in terms of providing the lowest VIN possible for highest efficiency to each charger while providing the proper output voltage. For example, the 2-cell charger would only require ~10VIN, while the 3-cell charger would only require ~14VIN. But, your overall system efficiency will hinge on how well the front-end flyback is designed.
     
    For your proposed approach with 5-cells all in one pack, you could certainly still use LTC4008. Again, Ryszard is correct in identifying the difference—or similarity, rather—between LTC4007 & LTC4008. However, we don’t recommend LTC4006/7 for anything beyond 2-4 series cell stacks; LTC4008 has a resistor adjustable output up to 6 cells and beyond. As I said, this approach requires cell balancing and since this is a step-down topology (buck), you’d always need VIN>VBAT, which is ~22VIN for headroom above the 21VBAT. LTC4009CUF-2#PBFLTC4009CUF-2#PBF & LTC4012 (recommended for higher current >4A) are also options, though you would need separate microcontroller connections for timer and thermal-qualified termination.
     
    For Li-ion batteries, the temperature is very stable during the entire charge cycle, but temperature failsafes are required for charging either below or above the manufacturer recommended temperature range. Termination for Li-ion/poly/FePO4 chemistries are all the same: timer or current-threshold (C/x). Most times a C/x termination is sufficient as the remaining time spent charging the battery from ~90-95 up to 100% is almost as long as the first 95%.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Mike,

    You are very wellcome of course, as you said, there is a border-line when 5-cells Li-Ion packs are needed.

    Aeromodelism shops sells 5 cell packs (cant remember the brand) but without any protection or cell balancing. By the way, we can find up to 4-cell packs with cell balancing and protection circuit (OVP) included.

    The only reasonable way I have found for getting 5-cell packs with protection and balance circuit included is directly from Tenergy. Problem is that price goes higher (and shipment from EEUU is expensive too).

     

    This is required for geotecnic applications. We sell pressuremeter probes for Spain that needs 18-24 VDC for operation. What we design is the equipment needed for reading the values, power the probe, computer connection through USB and software. All included in one case with batteries inside, as this is usually used for fieldworks.

    We have jumped from Lead-Acid to Li-Ion recently. Then number of units we sell per year it´s linked to the activity of geotecnic companies here in Spain. So it´s for low-volume consumer of course.

    I would have designed a step-up converter from a 4-cell pack, but I would like to avoid it because of the noise it can spread around the pcb and of course, the efficiency lost.

     

    For the moment the only quality choice I have seen for the 5-cell pack is buying directly to Tenergy or a Tenergy-reseller who has bought a high quantity of this 5-cell Tenergy packs. I remember that Farnell told me that their products availability depends on the demand... I would be glad to hear alternatives for Europe. Thank you very much for your lines.

     

    Best Regards,

     

    Cristian,

    NDT Ingenieros S.L.

    Spain

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    Hi Cristian,

     

    fo small quantity you can build your own pack using e.g. bq77910 protection/balancing IC:

    http://www.ti.com/product/bq77910