Power & Energy
  • Technologies
  • More
Power & Energy
Forum Maximising power output from solar panels
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 290 subscribers
  • Views 2821 views
  • Users 0 members are here
  • micro-inverter
  • solar_tracker
  • micro_inverters
  • mppt
  • solar
  • tracking_systems
Related

Maximising power output from solar panels

Former Member
Former Member over 13 years ago

There is an ongoing debate in the sector about how best to maximise the power from a solar panel and minimise shading effects: do you use a micro-inverter with built in MPPT or do you use a solar tracker. Both have cost implications, but what is your preference from a technical viewpoint?

  • Sign in to reply
  • Cancel

Top Replies

  • Catwell
    Catwell over 13 years ago +1
    Although I am not in the alternative energy industry, I would have to lean towards the MPPT option. For stationary panels, the MPPT option is best for choosing the best location for maximum output. However…
  • Former Member
    Former Member over 12 years ago in reply to bad_boy_y +1
    Sounds good to me, but the amount of copper would be more to use 12v since you lose more power in the line for a given power transmission. Think about it, to send 100watts through the line you would need…
  • sbkenn
    0 sbkenn over 12 years ago in reply to smartengineer

    Cooled to what ?  Kelvin is the relevant scale.  Cooling by 10C is going to use more energy than you gain from the PV.

    On another point, that of MPPT, I suggest that, in order to charge batteries to the maximum, the PV would need to charge a large capacitor, then through a buck-boost converter, so that even in low light conditions, some power would be acquired.  The converter would determine where the MPP is, and draw current from the PV/capacitor into the the batteries to meet MPP requirements.

    Plain ol' PWM won't do that, regardless of it's intelligence.  This is particularly relevant where average light isn't great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • donn18013
    0 donn18013 over 12 years ago in reply to Former Member

    To transport power, it is still necessary to convert to AC. The battle between Edison and Tesla was over a hundred years ago, Tesla (and Westinghouse) won. DC is ok for short distances - like the length of a car - but not for transporting through the grid. But I do agree, solar is the future.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nihaomike
    0 nihaomike over 11 years ago in reply to sbkenn

    A big capacitor is not necessary. In low light, just slow down the charging. That does mean that many off the shelf charger chips are not suitable for this use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Regardless of the mechanism for concentration of solar input, dust and other barrier particulate materials will degrade you power output over the long term - particularly when you rely on a protective covering for the PV panels that can be affected by the environment (pitting, oxidation, etc) that decreases your output. For traditional PV panels, cooling the substrate will allow for thermo-voltaic conversion while simultaneously improving the PV panel's output for the same input radiance. I used this process with submerged flexible panels in the Solar Seaweed design, which was intended to also use piezoelectric film to capture wave energy as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<