Power & Energy
  • Technologies
  • More
Power & Energy
Forum Best, most efficient way to get 5WDC from 120VAC 60Hz
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 284 subscribers
  • Views 800 views
  • Users 0 members are here
  • current
  • ac-dc
  • power_management
  • converter
  • Design
  • power_supply
  • power_conversion
  • power
  • energy
  • regulator
Related

Best, most efficient way to get 5WDC from 120VAC 60Hz

nathanjseeley
nathanjseeley over 13 years ago

First off, Not sure if this is the right place to be posting this, but I need help.

 

So I am working on making some phone chargers (my friend is knitting the "enclosures" for them, they are really cute) I am looking for the best way to take Standard US Household voltage and drop it to +5VDC.

 

I have two thoughts and am wondering which would be the best.

 

1. Use a chain of voltage regulators and a rectifying bridge to drop the voltage (more heat, possibly less weight)

 

2. Use a transformer to drop it from 120VAC to 12VAC then put it through the bridge and a 5V regulator (less heat, possibly heavier)

 

Which of these methods would you guys suggest, also is there going to be more to the circuit than just the Transformers, regulators and their associated hardware?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Best, most efficient way would be to build a switch mode power supply by rectifying your ac directly to +/- 170 volts dc, then using a control unit turn it back to Ac at about 100 KHz or higher. This would…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Use one of those "cute" 120VAC to USB power supplies cubes, like those provided for an iPad mini. All USB ports have a +5 volt power capability. I saw them at the Walgreens checkout for cheap. Plug your phone into a USB port on a computer and you can borrow the +5 volts from it as well.

     

    The simplest way to convert 120 VAC to +5 volts is a capacitor. Use it to drop the voltage to a zener regulator. You didn't say how much current. This technique is for low current, non-line isolated applications. Nobody is to come in contact with either lead of this supply for safety reasons.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Use one of those "cute" 120VAC to USB power supplies cubes, like those provided for an iPad mini. All USB ports have a +5 volt power capability. I saw them at the Walgreens checkout for cheap. Plug your phone into a USB port on a computer and you can borrow the +5 volts from it as well.

     

    The simplest way to convert 120 VAC to +5 volts is a capacitor. Use it to drop the voltage to a zener regulator. You didn't say how much current. This technique is for low current, non-line isolated applications. Nobody is to come in contact with either lead of this supply for safety reasons.