Power & Energy
  • Technologies
  • More
Power & Energy
Forum Best, most efficient way to get 5WDC from 120VAC 60Hz
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 284 subscribers
  • Views 802 views
  • Users 0 members are here
  • current
  • ac-dc
  • power_management
  • converter
  • Design
  • power_supply
  • power_conversion
  • power
  • energy
  • regulator
Related

Best, most efficient way to get 5WDC from 120VAC 60Hz

nathanjseeley
nathanjseeley over 13 years ago

First off, Not sure if this is the right place to be posting this, but I need help.

 

So I am working on making some phone chargers (my friend is knitting the "enclosures" for them, they are really cute) I am looking for the best way to take Standard US Household voltage and drop it to +5VDC.

 

I have two thoughts and am wondering which would be the best.

 

1. Use a chain of voltage regulators and a rectifying bridge to drop the voltage (more heat, possibly less weight)

 

2. Use a transformer to drop it from 120VAC to 12VAC then put it through the bridge and a 5V regulator (less heat, possibly heavier)

 

Which of these methods would you guys suggest, also is there going to be more to the circuit than just the Transformers, regulators and their associated hardware?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Best, most efficient way would be to build a switch mode power supply by rectifying your ac directly to +/- 170 volts dc, then using a control unit turn it back to Ac at about 100 KHz or higher. This would…
Parents
  • ChuckMcM
    0 ChuckMcM over 13 years ago

    You need to define "best". If you want it small and cheap then rectifying the AC to a capacitor/inductor and using a FET to switch the volts on and off to the capacitor. Since you're only at 5V you can get away with halfwave rectifying the AC if you're going to draw < 5W.  You can almost get this 'off the shelf' with a Maxim chip. This is the 'cheap USB recharger' that sells for about $1.50 each on places like Alibaba. But if 'best' includes (won't start a fire when the transistor fails) you might want to stay away from those.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ChuckMcM
    0 ChuckMcM over 13 years ago

    You need to define "best". If you want it small and cheap then rectifying the AC to a capacitor/inductor and using a FET to switch the volts on and off to the capacitor. Since you're only at 5V you can get away with halfwave rectifying the AC if you're going to draw < 5W.  You can almost get this 'off the shelf' with a Maxim chip. This is the 'cheap USB recharger' that sells for about $1.50 each on places like Alibaba. But if 'best' includes (won't start a fire when the transistor fails) you might want to stay away from those.