Power & Energy
  • Technologies
  • More
Power & Energy
Forum I need help designing a 400hz 115vac 3phase power supply -- Help
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 32 replies
  • Answers 3 answers
  • Subscribers 285 subscribers
  • Views 11740 views
  • Users 0 members are here
  • power_management
  • 400hz
  • power_supply
  • power_conversion
Related

I need help designing a 400hz 115vac 3phase power supply -- Help

phoenixcomm
phoenixcomm over 13 years ago

Hi I need to find a way to get 400hz/115vac/3phase cheaply..  Im a digital person...

any thoughts.

The unit could be powered from a 28vdc source but better yet 115ac house hold 15amp circuit

 

 

Cris

  • Sign in to reply
  • Cancel

Top Replies

  • artful_bodger
    artful_bodger over 11 years ago +3
    If you are borrowing mil spec gear, they will not want it damaged, so you'll need to read the relevant spec and understand how to contain your supply within the spec. Too many harmonics and you'll most…
  • billabott
    billabott over 13 years ago +1
    Could this be what you had in mind? http://www.newark.com/schneider-electric/atv12h037m3/ac-drive/dp/11R1086
  • michaelkellett
    michaelkellett over 13 years ago in reply to phoenixcomm +1
    Hello Cristina, I could give you some assistance but first I would need to know what you want to drive with it and what other constraints you have. This is not a simple project and if you only want one…
Parents
  • peterjcs23
    0 peterjcs23 over 10 years ago

    or, if you wanted something very simple, you've been suggesting an Arduino solution, you could derive a 3 phase logic signal with 3 logic pins and apply them to a  high voltage opamp on each phase via AC coupling and a bit of filtering. (The supply would have to provide current limit.)

    image

    Once you got this working you could boost the voltage too on the output stage.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • AK7466
    0 AK7466 over 5 years ago in reply to peterjcs23

    Hi.

     

    Like so many before me I am try to build 3 phase 115v, 400Hz supply to drive an ex-aircaft gyroscope (or two).

     

    My starting point is this ready made module

    http://www.bldcmotor-driver.com/sale-11361290-110v-220v-ac-input-stepper-motor-driver-board-high-voltage-motor-control-board.html

     

    which comprises a JY02A Sensorless brushless DC motor control IC

    https://docplayer.net/146908738-Jy02a-sensorless-brushless-dc-motor-control-ic.html

     

    and a JY213 Motor Driver MOSFET / IGBT Driver High Speed 3 - Phase Half - Bridge

    http://www.bldcmotor-driver.com/sale-11344385-jy213h-bldc-motor-driver-mosfet-igbt-driver-high-speed-3-phase-half-bridge.html

     

    To give these old gyros the easiest possible life I would like the drive waveforms to be as close to sinusoidal as is realisticaly possible so I am envisgaing incorporating 400 Hz L/C low pass filters between the output of the drivers and the gyro windings.

     

    I have looked at various LC filter design tools such as

     

    PI Filter      http://www.calculatoredge.com/electronics/ch%20pi%20low%20pass.htm

    Chebyshef  https://rf-tools.com/lc-filter/

     

    and understandably all of these design tools require a source and load impedances to be specified.

     

    In my application the source impedance will hopefully be very low, and I have no idea what the gyro winding impedance will be when rotating.

     

    Please can somebody suggest the best way forward, or point me in the direction of some helpful documentation?

     

    Many thanks

     

    Alan K. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to AK7466

    Hi Alan,

     

    I think it's not required, an example is BLDC motors themselves, they are expensive but do not get damaged by electronic switching of voltage across the windings. Same with hobby CNC that uses stepper motors. PWM'ing of motors is very common too, although that's at a higher frequency. The current will change linearly through the coil windings due to their inductance, and this will self-smooth. If it doesn't, you can add an extra inductance in series with the winding.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • AK7466
    0 AK7466 over 5 years ago in reply to shabaz

    Hi Shabaz.  Thank you for your thoughts and comments, and taking the trouble to respond.

     

    As you say, I can add an extra inductance in series with the winding.

    What I would like to know is how to calculate the optimum value for the inductance, and whether it would also be beneficial to add a capacitor as well?

     

    Thanks again

     

    Alan K.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • AK7466
    0 AK7466 over 5 years ago in reply to shabaz

    Hi Shabaz.  Thank you for your thoughts and comments, and taking the trouble to respond.

     

    As you say, I can add an extra inductance in series with the winding.

    What I would like to know is how to calculate the optimum value for the inductance, and whether it would also be beneficial to add a capacitor as well?

     

    Thanks again

     

    Alan K.