Power & Energy
  • Technologies
  • More
Power & Energy
Forum Exercise Bike Generator
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 283 subscribers
  • Views 992 views
  • Users 0 members are here
Related

Exercise Bike Generator

e14 Contributor
e14 Contributor over 13 years ago

I have an 11-year-old son who is overweight; he enjoys games on the computer.  I have a plan to hook his computer monitor up to a generator attached to an exercise bike so that if he wants to see what's going on, he has to pedel.  The monitor is a 12V 3amp monitor.  I am totally new to electronics (I am learning about voltage, ams, current, regulators, capacitors, etc.).  I understand I need a 12v generator.  I, also, understand I need some way to control the voltage, amps, etc. (whatever ?) going from the generator to the monitor (a regulator ?).  Obviously, the pedel rotation speed will vary; but I need a constant output to the monitor.  Also, if he pedels too slow, the monitor will go off (the computer will be plugged into AC current -- so the computer won't shut down if he stops pedeling).  How do I set this up?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,

    It is gives more efficiency if you can charge the separate battery from the coupled DC generator to the bike rather than try to control directly your applications.

    Measure the voltage output from the DC generator and if it is enough to charge Battery then gives a signal to turn on the Monitor power supply.If low turn off the supply.

     

    Mechanical relay or Trac can be used to switching application.

     

    Microcontroller or Logic circuit can be designed to sense the voltage readings.

     

    From that you can use Battery power to DC light system, USB power and what u need. You can also do invert it to 230 v.

     

    You can find the data from energy guide what should be the RPM for better calories burning and from that you can sense the RPM and design controlling according to RPM.

     

    RPM can be sense DC Generator back EMF Energy calibration or other sensors.

    image

    Thanks

    Tharindu Chandimal

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,

    It is gives more efficiency if you can charge the separate battery from the coupled DC generator to the bike rather than try to control directly your applications.

    Measure the voltage output from the DC generator and if it is enough to charge Battery then gives a signal to turn on the Monitor power supply.If low turn off the supply.

     

    Mechanical relay or Trac can be used to switching application.

     

    Microcontroller or Logic circuit can be designed to sense the voltage readings.

     

    From that you can use Battery power to DC light system, USB power and what u need. You can also do invert it to 230 v.

     

    You can find the data from energy guide what should be the RPM for better calories burning and from that you can sense the RPM and design controlling according to RPM.

     

    RPM can be sense DC Generator back EMF Energy calibration or other sensors.

    image

    Thanks

    Tharindu Chandimal

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thank you for your response.

    I am reluctant to use a battery because my purpose is to have my son pedel while hs is playing games; if I use a battery, he can stop pedeling once the battery is charged.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I was just re-reading your post and looking at your diagram -- it appears I may have misunderstood what you are suggesting.

     

    From what I think you are saying, I could, simply, use a switch which allows current to pass to the monitor.

     

    So, can I just plug the monitor into the AC house current and use the provided transformer to turn on the monitor.  Then, have an On/Off switch (a relay switch ?) which allows the current to pass on to the monitor if the pedels are moving; but, if my son stops pedeling, the switch would open the circuit and prevent the passage of current to the monitor?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    Hi Richard,

     

    Here's a quick way to achieve the goal but is a different manner:

    1. Get a bicycle dynamo, and assuming you can mechanically connect it to the excercise bike

    2. Get a 12V relay, and connect the dynamo to the 'coil' pins on the relay

    3. Find a monitor cable that you don't mind destroying, and find a wire in there that if you break, will cause the image to disappear. Once you've found it, connect up two pins on the relay to the two wire breaks. Connect the 'Common' pin of the relay to one break, and the 'normally open' end to the other. Keep wiring short here, otherwise you could cause a poor image, or no image at all.

     

    This method requires very little electronics knowledge, and is safer than connecting to the mains. Others may have different ideas.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    The exercise bike has a speed indicator (based upon a magnet on the wheel which passes a sensor on each revolution of the wheel).  I think I can use the speed indicator to monitor the speed -- this information would, then, be used to activate a relay switch to close a circuit if the speed is at a certain minimum setting.