Power & Energy
  • Technologies
  • More
Power & Energy
Forum Raising the voltage to use a photocell
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 35 replies
  • Answers 1 answer
  • Subscribers 288 subscribers
  • Views 4143 views
  • Users 0 members are here
  • solar-powered
  • Alternative Energy Tags
Related

Raising the voltage to use a photocell

Former Member
Former Member over 11 years ago

Anyone know how can i raising the voltage of a photocell?, from 0.5 volts to 5 volts, the photocell give me 0.5 volts and 9 amp, the problem is that if i use operational amplifier, i don't have the power to energize a small engine, i appreciate any information that  could be usefull or component that resist the power.image

¿Alguien sabe como puedo utilizar esta celda solar?, entrega 0.5 v y 9 amp, por ende la potencia es de 4.5 Watts, necesito subir el voltaje a 5 V aunque se reduzca la corriente, pero los diseños con operacionales no me resultan funcionales ya que tendria que darme alrededor de medio amper, y no resisten la corriente, ¿tienen alguna idea de como puedo hacerlo?

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    0 mcb1 over 11 years ago

    Have you measured the voltage and current to be sure.

    0.5v at 9 Amps = 4.5w and most panels of this output power usually are of a higher voltage like 12v or even some at 6v.

     

    Is there any specifications for it.? (I did see there were no labels visible in the pictures)

     

    I think your best option is to replace it with something of a similar size but a more user friendly voltage.

     

    Mark

    -------------------

     

    ¿Ha medido el voltaje y la corriente para estar seguro.
    0.5v a las 9 Amperios = 4.5W y la mayoría de los paneles de esta potencia de salida por lo general son de un voltaje más alto como 12 o incluso algunos en 6v.

    ¿Hay alguna especificación para ello.? (Que yo realmente vi que no había etiquetas visibles en las imágenes)

    Creo que su mejor opción es reemplazarlo con algo de un tamaño similar pero un voltaje más amigable.

    Marca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to mcb1

    Sounds more like a single cell voltage Mark. either he's going to need more cells to get a working voltage or use a Switch mode boost converter to jack it up to something useful. Quite likely a combination of both of those will be the best.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 11 years ago in reply to mcb1

    Sounds more like a single cell voltage Mark. either he's going to need more cells to get a working voltage or use a Switch mode boost converter to jack it up to something useful. Quite likely a combination of both of those will be the best.