Power & Energy
  • Technologies
  • More
Power & Energy
Forum Replacing battery charger diodes
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 286 subscribers
  • Views 4467 views
  • Users 0 members are here
Related

Replacing battery charger diodes

e14 Contributor
e14 Contributor over 11 years ago

I have 6 and 10 amp, 12 volt manual automotive type battery chargers with bad diodes. These diodes are mounted on an aluminum plate.

I am looking at replacing these diodes with stud mount diodes, style DO4/DO5 etc. I have used MUR2515 in the past, but 1 of these has blown when hooked up to a very dead battery.

I was looking at purchasing MUR2510, 25F40 or FR30G02 as replacements.

Would these be suitable replacements and should I stick with fast recovery diodes?

Any suggested diode #s are appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +1
    You don't need a fast diode for this. I'd get power diodes rated at least about twice the nominal current capacity of your chargers. I'd be looking at ones that had a BV of at least 50 volts. Shottktys…
Parents
  • kidiccurus
    0 kidiccurus over 11 years ago

    Just find diodes with the same part numbers as the original and replace like for like.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kidiccurus

    That would just be too easy.

    There are no #'s on them.

    I also want to get rid of the "button" style of diodes and replace then with ones that are easier to change in case of failures.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kidiccurus

    That would just be too easy.

    There are no #'s on them.

    I also want to get rid of the "button" style of diodes and replace then with ones that are easier to change in case of failures.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • supper_slash
    0 supper_slash over 11 years ago in reply to e14 Contributor

    Send a pic of the diodes please

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to supper_slash

    I will try to upload a pic of the old rectifier plate with button diodes.

    In the back is the charger with stud style diodes installed on another plate.