Power & Energy
  • Technologies
  • More
Power & Energy
Forum 120v led lamp
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 3287 views
  • Users 0 members are here
Related

120v led lamp

moelleux
moelleux over 11 years ago

Hi,

Ive just started hacking electronics lately, thanks to Jeremy Blum book and tutorials!

 

My desk lamp fluorescent bulb gave up on me and i wanted to replace the bulb with some white LEDs.  So i took appart the lamp and found a circuit board and im not sure what it is for. The fluorescent bulb is rated 120V and i tought it was directly hooked to AC? is this board an AC to DC converter?

Heres some pictures (The side with the fuse is the 120v AC in) :

20141030083725 - HostingPics.net - Hébergement d'images gratuit

20141030083741 - HostingPics.net - Hébergement d'images gratuit

20141030083754 - HostingPics.net - Hébergement d'images gratuit

20141030083813 - HostingPics.net - Hébergement d'images gratuit

 

So my plan is to enclose a AC to DC converter to a potentiometer that would feed current to around 20 white LEDs(maybe those MCL034SWC-YH1MCL034SWC-YH1. This is my main light source in that room so i would like it to be very bright, but dimmable.
Thanks!

Feel free to recommend me stuff!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago in reply to supper_slash +2
    Hi Lupe, Not sure that circuit will work, unless there is something I don't understand about the 555 (quite likely). Anyway, there is a great resource here, with plenty of 555 circuits - including PWM…
  • jw0752
    jw0752 over 11 years ago in reply to moelleux +1
    Hi William, I also wanted to make sure you used 100 nF caps where indicated. These are also labeled 0.1 uF. If we get the capacitance too high we lower the frequency of the 555 which would allow you to…
  • moelleux
    moelleux over 10 years ago +1
    It's been a while, but i thought i would share it anyway. I've been using it for almost a year now and it's great lighting. Especially for phone repair and precision stuff. I made 2 versions of the board…
Parents
  • moelleux
    0 moelleux over 11 years ago

    I finally got some stuff done! I made the exact same thing as below with a 15v psu. Everything seem fine except the leds are blinking quickly instead of dimming. I tryed adding 470uf caps but it dont seem like doing anything.. would i need a larger cap? or maybe its the 555 that would need adjustment to run 15v?

     

    PWM-Controller.gif

    any idea would be appreciated

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to moelleux

    Hi William, I also wanted to make sure you used 100 nF caps where indicated. These are also labeled 0.1 uF. If we get the capacitance too high we lower the frequency of the 555 which would allow you to see the  effect of the PWM. I do not think that the 15 volts is the problem as the 555 is designed to run at that voltage. Let me know how it works out.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to moelleux

    Hi William, I also wanted to make sure you used 100 nF caps where indicated. These are also labeled 0.1 uF. If we get the capacitance too high we lower the frequency of the 555 which would allow you to see the  effect of the PWM. I do not think that the 15 volts is the problem as the 555 is designed to run at that voltage. Let me know how it works out.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • moelleux
    0 moelleux over 11 years ago in reply to jw0752

    Thanks for the advice, now it works perfect.
    i tryed 56nF but it was still flickering a little.  Then i tryed 33pF and it cant be noticed anymore.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 11 years ago in reply to moelleux

    Keep up the great work John.