Power & Energy
  • Technologies
  • More
Power & Energy
Forum Flashing LED with 555 timer
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 6346 views
  • Users 0 members are here
  • power_management
Related

Flashing LED with 555 timer

e14 Contributor
e14 Contributor over 11 years ago

Hello all,

 

I am trying to create a flashing 3 LED circuit with a 9v battery. I want a specific flash time of 20ms and a duty cycle of 1.3 seconds. My question is what size should R1, R2, and C1 be in order to achieve that timing. I found the equations for figuring it out, I was hoping maybe someone would rather take the challenge of giving me the answer instead of me going back to school to relearn algebra. Any help is very much appreciated.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Rob, Without a schematic to reference no one will be able to figure those values for you. Just in case you are looking for a good 555 reference here is an online book one of the guys showed me a while…
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor +1
    Hi Rob, paulellison is correct that what you want to do might be easier to accomplish with a microprocessor. Also for the 5 volt power you are showing on your schematic you will probably not be able to…
  • D_Hersey
    D_Hersey over 11 years ago +1
    Hi John, I'll have you know that on the morning of the Packer's victory over the Cowboys, I had Kielbasa con chilaquiles for breakfast in support of their effort. They were tasty, I admit. I'm sure it…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Rob, Without a schematic to reference no one will be able to figure those values for you. Just in case you are looking for a good 555 reference here is an online book one of the guys showed me a while back.

     

    http://www.talkingelectronics.com/projects/50%20-%20555%20Circuits/50%20-%20555%20Circuits.html#9A

     

    You can vary the percentage of on to off time with this circuit. You will have to experiment to get it to the frequency where you want it.

    John 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    image

    Thank you for the quick reply Mr. John and Mr. Paul.

     

    Here is the circuit that I came up with. I am shooting for a 20ms time high with a 1.3 Second cycle time. I found an online calculator at 555 Astable Circuit Calculator

    but its very confusing to me at this point. When I change one value it seems to change others throwing me way off. I can't keep up with it. If any of you gentlemen have a better suggestion for me on this circuit I'm listening. Also thanks for the link Mr. John that will be very helpful in my future projects. Also a quick correction. It will be powered with a 9v Battery, not 5 volts as pictured above.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Hi Rob.

     

    Thanks for your diagram.

     

    I have also visited the page you referenced. The calculator (annoyingly) works based on submitted component values rather than timings, the reverse to what you really need. An interesting point I did take from this page is as follows:

    In this type of circuit, the duty cycle can never be 50% or lower.

     

    The following page goes on to say: http://www.daycounter.com/Calculators/NE555-Calculator.phtml

    Note that the minimum duty cycle is 50 percent, so if you need a smaller duty cycle you need to use an inverter on the output. 

    I don't really have much 555 Timer experience, but from what i have read, this would seem to apply to you.

     

    At this point I would probably put an extra 30p into the project and use an AtTiny85 instead. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Hi Rob.

     

    Thanks for your diagram.

     

    I have also visited the page you referenced. The calculator (annoyingly) works based on submitted component values rather than timings, the reverse to what you really need. An interesting point I did take from this page is as follows:

    In this type of circuit, the duty cycle can never be 50% or lower.

     

    The following page goes on to say: http://www.daycounter.com/Calculators/NE555-Calculator.phtml

    Note that the minimum duty cycle is 50 percent, so if you need a smaller duty cycle you need to use an inverter on the output. 

    I don't really have much 555 Timer experience, but from what i have read, this would seem to apply to you.

     

    At this point I would probably put an extra 30p into the project and use an AtTiny85 instead. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to gadget.iom

    Something like this should handle your output inversion.

    74AHC1G04GW,125 - NXP - INVERTER GATE, SINGLE, TSSOP-5 | Farnell element14