Power & Energy
  • Technologies
  • More
Power & Energy
Forum Flashing LED with 555 timer
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 285 subscribers
  • Views 6202 views
  • Users 0 members are here
  • power_management
Related

Flashing LED with 555 timer

e14 Contributor
e14 Contributor over 11 years ago

Hello all,

 

I am trying to create a flashing 3 LED circuit with a 9v battery. I want a specific flash time of 20ms and a duty cycle of 1.3 seconds. My question is what size should R1, R2, and C1 be in order to achieve that timing. I found the equations for figuring it out, I was hoping maybe someone would rather take the challenge of giving me the answer instead of me going back to school to relearn algebra. Any help is very much appreciated.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Rob, Without a schematic to reference no one will be able to figure those values for you. Just in case you are looking for a good 555 reference here is an online book one of the guys showed me a while…
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor +1
    Hi Rob, paulellison is correct that what you want to do might be easier to accomplish with a microprocessor. Also for the 5 volt power you are showing on your schematic you will probably not be able to…
  • D_Hersey
    D_Hersey over 11 years ago +1
    Hi John, I'll have you know that on the morning of the Packer's victory over the Cowboys, I had Kielbasa con chilaquiles for breakfast in support of their effort. They were tasty, I admit. I'm sure it…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Rob, Just for the fun of it I mocked up your idea using an Arduino Duemilanove. I will attach a video but keep in mind that my camera has a slow scan rate and as such it misses the 20 uS flash occasionally. In real life the 3 LEDs flash for 20 uS and then are off for 1.3 seconds before they flash again. The camera misses every third of fourth flash. I have taken the simplest of Arduino sketches called "Blink" and modified it to your specifications of 20 uS on and 1.3 Seconds off. The Arduino outputs this signal on pin 12 in this case and I am using the signal to trigger an NTD4906 gate level N channel MOSFET. I am supplying 9 volts to the LEDs and the FET so there is enough voltage to drive them in series and there is also a 220 ohm current limiting resistor in series. I do not know the intention of your project whether you need this effect or if you are just trying to learn about the 555.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    Hi Rob, Just for the fun of it I mocked up your idea using an Arduino Duemilanove. I will attach a video but keep in mind that my camera has a slow scan rate and as such it misses the 20 uS flash occasionally. In real life the 3 LEDs flash for 20 uS and then are off for 1.3 seconds before they flash again. The camera misses every third of fourth flash. I have taken the simplest of Arduino sketches called "Blink" and modified it to your specifications of 20 uS on and 1.3 Seconds off. The Arduino outputs this signal on pin 12 in this case and I am using the signal to trigger an NTD4906 gate level N channel MOSFET. I am supplying 9 volts to the LEDs and the FET so there is enough voltage to drive them in series and there is also a 220 ohm current limiting resistor in series. I do not know the intention of your project whether you need this effect or if you are just trying to learn about the 555.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    John