Power & Energy
  • Technologies
  • More
Power & Energy
Forum Flashing LED with 555 timer
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 286 subscribers
  • Views 6172 views
  • Users 0 members are here
  • power_management
Related

Flashing LED with 555 timer

e14 Contributor
e14 Contributor over 11 years ago

Hello all,

 

I am trying to create a flashing 3 LED circuit with a 9v battery. I want a specific flash time of 20ms and a duty cycle of 1.3 seconds. My question is what size should R1, R2, and C1 be in order to achieve that timing. I found the equations for figuring it out, I was hoping maybe someone would rather take the challenge of giving me the answer instead of me going back to school to relearn algebra. Any help is very much appreciated.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Rob, Without a schematic to reference no one will be able to figure those values for you. Just in case you are looking for a good 555 reference here is an online book one of the guys showed me a while…
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor +1
    Hi Rob, paulellison is correct that what you want to do might be easier to accomplish with a microprocessor. Also for the 5 volt power you are showing on your schematic you will probably not be able to…
  • D_Hersey
    D_Hersey over 11 years ago +1
    Hi John, I'll have you know that on the morning of the Packer's victory over the Cowboys, I had Kielbasa con chilaquiles for breakfast in support of their effort. They were tasty, I admit. I'm sure it…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Mr. John,

    Thank you you for the video. I have tried the same on my Arduino Uno. I guess I should go into more detail as to why I am trying to achieve this effect and on what platform. During my time in the military we used IR strobes in order to ID one another on the ground at night. Through night vision goggles these things are super bright. I actually still have two of them hidden somewhere in my house. One has two probes sticking out that you make contact with them with something conductive to program different flashes The other more simple is set on a fixed time. I can't find them. Here is a link to the exact strobes among others that we used.

    https://www.cejayengineering.com/Buy-Online/IR-Strobes-Beacons/902111IR.html

    I Wanted to try and recreate the circuit in order to use different color LEDs and to learn more about the 555. Every circuit I come up with looks more like a dim light blinking instead of the bright strobe effect that these small strobes produce. I tried to find the ones that I have in order to see what was inside but have had no luck finding them. I looked at there website to see the data sheet and all it really gives is the timing of it. So that's why I have been shooting for that particular timing. If I can figure it out i want to get a bunch of boards printed so that I can make different colors and give them to all the kids in my family. Just something neat to play with and drive there parents crazy. Plus I have a bit of kid left in me as well. I just wanted to see how hard/easy cheap or expensive that I could build them for really.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Mr. John,

    Thank you you for the video. I have tried the same on my Arduino Uno. I guess I should go into more detail as to why I am trying to achieve this effect and on what platform. During my time in the military we used IR strobes in order to ID one another on the ground at night. Through night vision goggles these things are super bright. I actually still have two of them hidden somewhere in my house. One has two probes sticking out that you make contact with them with something conductive to program different flashes The other more simple is set on a fixed time. I can't find them. Here is a link to the exact strobes among others that we used.

    https://www.cejayengineering.com/Buy-Online/IR-Strobes-Beacons/902111IR.html

    I Wanted to try and recreate the circuit in order to use different color LEDs and to learn more about the 555. Every circuit I come up with looks more like a dim light blinking instead of the bright strobe effect that these small strobes produce. I tried to find the ones that I have in order to see what was inside but have had no luck finding them. I looked at there website to see the data sheet and all it really gives is the timing of it. So that's why I have been shooting for that particular timing. If I can figure it out i want to get a bunch of boards printed so that I can make different colors and give them to all the kids in my family. Just something neat to play with and drive there parents crazy. Plus I have a bit of kid left in me as well. I just wanted to see how hard/easy cheap or expensive that I could build them for really.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi Rob, Thanks for the insight into your project. This is off subject but Robert Peter Oakes showed me a while ago that one can see the infrared LEDs using a camera on a cell phone or other camera. Try it with your TV remote control. I will let you know if I can come up with any other simple circuits.

    John