Power & Energy
  • Technologies
  • More
Power & Energy
Forum Flashing LED with 555 timer
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 286 subscribers
  • Views 6143 views
  • Users 0 members are here
  • power_management
Related

Flashing LED with 555 timer

e14 Contributor
e14 Contributor over 11 years ago

Hello all,

 

I am trying to create a flashing 3 LED circuit with a 9v battery. I want a specific flash time of 20ms and a duty cycle of 1.3 seconds. My question is what size should R1, R2, and C1 be in order to achieve that timing. I found the equations for figuring it out, I was hoping maybe someone would rather take the challenge of giving me the answer instead of me going back to school to relearn algebra. Any help is very much appreciated.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Rob, Without a schematic to reference no one will be able to figure those values for you. Just in case you are looking for a good 555 reference here is an online book one of the guys showed me a while…
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor +1
    Hi Rob, paulellison is correct that what you want to do might be easier to accomplish with a microprocessor. Also for the 5 volt power you are showing on your schematic you will probably not be able to…
  • D_Hersey
    D_Hersey over 11 years ago +1
    Hi John, I'll have you know that on the morning of the Packer's victory over the Cowboys, I had Kielbasa con chilaquiles for breakfast in support of their effort. They were tasty, I admit. I'm sure it…
Parents
  • gihu
    0 gihu over 11 years ago

    Hi Rob,

     

    I don't know if you keep on wanting to try it with 555.

    If yes, try this sch.

    image

     

    See some rude calculations:

    image

    image

     

    But I am not sure if it is posible for the human eye seeing so short pulse, try it.

     

    Also take into account that timing may vary depending on the resistors and capacitor tolerance, if you are looking for accuracy just use microcontrollers as our colleagues suggest.

     

    Hope that helps,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to gihu

    Hi Gihu,

    For the fun I bread boarded your circuit and it seems to work just as you predicted. I couldn't quite get to the 18 meg value of Ra so it was flashing a little more often than 1.3 seconds. I ran the Vcc at 9 volts and used an NTE 29 equivalent for the output transistor. The duration of the pulse is not a problem for the human eye which can detect even one photon under proper circumstances. The problem is as soon as the pulse gets shorter than about 70 mS the eye continues to interpret the pulse as being 70 mS. This is because of the residual image effect of the photoreceptors in the eye. Here is a photo of my circuit.

    Rob should be able to use your design to do what he wants and the values that you have calculated are very close. I did not put the scope on them but from what I gather he may not be that critical for his application.

    John

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to gihu

    Hi Gihu,

    For the fun I bread boarded your circuit and it seems to work just as you predicted. I couldn't quite get to the 18 meg value of Ra so it was flashing a little more often than 1.3 seconds. I ran the Vcc at 9 volts and used an NTE 29 equivalent for the output transistor. The duration of the pulse is not a problem for the human eye which can detect even one photon under proper circumstances. The problem is as soon as the pulse gets shorter than about 70 mS the eye continues to interpret the pulse as being 70 mS. This is because of the residual image effect of the photoreceptors in the eye. Here is a photo of my circuit.

    Rob should be able to use your design to do what he wants and the values that you have calculated are very close. I did not put the scope on them but from what I gather he may not be that critical for his application.

    John

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • gihu
    0 gihu over 11 years ago in reply to jw0752

    Cool!!

    John, thanks for checking it!!  image