Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14714 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • mpulliam
    0 mpulliam over 6 years ago

    7812 voltage regulator test results:

    w/ Power off and writing facing me

    Black lead on the center pin, read lead on the left pin = 1.2mV and it trickled down to 0

    Black lead on the center pin, read lead on the right pin = .5mV and it trickled down to a negative number

     

    w/ Power On and writing facing me

    Black lead on the center pin, read lead on the left pin = 30V

    Black lead on the center pin, read lead on the right pin = 12.04v

     

    I re-tested the D313 for continuity (after the unit has been turned on and off)

    There is NO continuity between the base and the emitter or collector

    There IS continuity between the emitter and the collector

     

    I retested the corroded diode and it is ok.  The corrosion was giving me a bad reading previously but I scraped it off and the diode shows a voltage reading of .519v in one direction and nothing in the other.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    All sounds good and normal except the D313. We need to test that one out of circuit and verify if it is good or bad.

     

    At some point I mistyped Read when I meant to type Red. I mention it so that we don't start a new convention for what is the correct nomenclature.  Sorry about that. I always try to proofread but at 1:30 AM I may miss things.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    I am going to order a replacement,  according to the data sheets, the NTE152 is similar but has different voltage (90v min and max) while the D313 is 60v min and max)

     

    Does that make a difference?

     

    Thanks,

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    I ran another test with the D311

     

    With my multimeter set to the diode tester...

    With the negative lead on the base, I get no reading touching the emitter or collector

    With the positive lead on the base, I get a .578 reading touching the middle pin

    With the positive lead on the base, I get a .580 reading touching the right pin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    I ran another test with the 2N3055 NPN power transistors

     

    With my multimeter set to the diode tester...

    When either the negative or positive is on the base (blue), I get a reading that starts out .03 and rises to 1V between the base and both the collector (red) or the emitter (yellow)

    When either the negative or positive is on the collector, I get a reading of about .010 V between the emitter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    I ran another test with the 2N3055 NPN power transistors

     

    With my multimeter set to the diode tester...

    When either the negative or positive is on the base (blue), I get a reading that starts out .03 and rises to 1V between the base and both the collector (red) or the emitter (yellow)

    When either the negative or positive is on the collector, I get a reading of about .010 V between the emitter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    This is actually an improvement. Go for it.

    John