Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14658 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • mpulliam
    0 mpulliam over 6 years ago

    PS If you don't mind, could you point out in a picture the internal parts that are lethal?  Is this only when the power is on?

     

    Thanks,

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    The high voltage danger is from the power wires that come into the unit, go to the fuse, the switch and then to the primary of the transformer. Than should be all.

     

    As I mentioned the 7812 is not a transistor but a voltage regulator. The 12 Volts that you measured on the one LM741 indicates that the 7812 is probably working OK. Go back and review my instructions for testing the 7812 and you should be able to verify that it is OK. You will expect a voltage of about 15 to 18Volts on the left lead and 12 volts on the right one.

     

    The lead of the diode looks OK. The color that you see is just left over flux from the soldering.

     

    The readings on the D313 do not sound normal. I do not know how your continuity tester works for this test compared to my analog meter but the readings you got make me suspicious. Putting the positive lead of the tester on the base should give continuity to the emitter and collector. If you want you can remove the D313 from the circuit and have it tested outside the circuit. If you don't have somewhere locally where you can get it tested you could send it to me. A good substitute for this transistor is a universal replacement from NTE called NTE152NTE152. It is an NPN power Transistor.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    The high voltage danger is from the power wires that come into the unit, go to the fuse, the switch and then to the primary of the transformer. Than should be all.

     

    As I mentioned the 7812 is not a transistor but a voltage regulator. The 12 Volts that you measured on the one LM741 indicates that the 7812 is probably working OK. Go back and review my instructions for testing the 7812 and you should be able to verify that it is OK. You will expect a voltage of about 15 to 18Volts on the left lead and 12 volts on the right one.

     

    The lead of the diode looks OK. The color that you see is just left over flux from the soldering.

     

    The readings on the D313 do not sound normal. I do not know how your continuity tester works for this test compared to my analog meter but the readings you got make me suspicious. Putting the positive lead of the tester on the base should give continuity to the emitter and collector. If you want you can remove the D313 from the circuit and have it tested outside the circuit. If you don't have somewhere locally where you can get it tested you could send it to me. A good substitute for this transistor is a universal replacement from NTE called NTE152NTE152. It is an NPN power Transistor.

     

    John