Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14734 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • mpulliam
    0 mpulliam over 6 years ago

    7812 voltage regulator test results:

    w/ Power off and writing facing me

    Black lead on the center pin, read lead on the left pin = 1.2mV and it trickled down to 0

    Black lead on the center pin, read lead on the right pin = .5mV and it trickled down to a negative number

     

    w/ Power On and writing facing me

    Black lead on the center pin, read lead on the left pin = 30V

    Black lead on the center pin, read lead on the right pin = 12.04v

     

    I re-tested the D313 for continuity (after the unit has been turned on and off)

    There is NO continuity between the base and the emitter or collector

    There IS continuity between the emitter and the collector

     

    I retested the corroded diode and it is ok.  The corrosion was giving me a bad reading previously but I scraped it off and the diode shows a voltage reading of .519v in one direction and nothing in the other.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    All sounds good and normal except the D313. We need to test that one out of circuit and verify if it is good or bad.

     

    At some point I mistyped Read when I meant to type Red. I mention it so that we don't start a new convention for what is the correct nomenclature.  Sorry about that. I always try to proofread but at 1:30 AM I may miss things.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    Sorry, that was a typo.  I retested the D313 and got those readings.

     

    But I ordered a new D313 (now a NTE152)

     

    I put it in when it gets here and get back to you.  If it doesn't fix it then I'll work on the 2N3055s

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    Sounds good , let me know.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    I got the NTE152NTE152 transistor in and it tests exactly the same as the pulled D313 transistor.  So I'll put in the new NTE152NTE152 and pull the power transistors to test next...

     

    New Transistor

    No Continuity between any pins

    Continuity between middle pin and backboard

    With positive on pin 1 and negative on pin 2 = .578 V

    With positive on pin 1 and negative on pin 3 = .580 V

     

    Old Transistor

    No Continuity between any pins

    Continuity between middle pin and backboard

    Continuity between middle pin and backboard

    With positive on pin 1 and negative on pin 2 =  .580 V

    With positive on pin 1 and negative on pin 3 =  .585 V

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    Still a no go for Voltage

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    Hi Matt,

     

    Good job on replacing the D313. Even though that wasn't the problem you at least have one more thing checked off the list. When you test the output transistors I believe they will be 2N3055. An NTE equivalent is an NTE130NTE130.

    Here is a picture of the pin out and the voltage I would expect from a diode check. On these it might also be good to check continuity especially between the Emitter and Collector. The resistance should be high in both polarities. Notice that the Emitter and Base is off center. With the Emitter and Base closer to the bottom of the picture the leads are identified as in the picture.

     

    image

     

    Based on how the unit is acting I am doubtful that these are going to be the problem but we must be sure. I am also a little at loss as to what to focus on next. Without a schematic I am not sure how the circuit is designed and my usual procedure for testing beyond the basics that we have done usually relies on tracing circuits and reverse engineering. These will be next to impossible to do remotely using only pictures. I will be thinking and you can let me know when you have tested the 2N3055s.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    Yep, correct on the Power Transistor. Hopefully I won't have to disconnect the blue and yellow wires.  If so, I'm not sure how to reconnect without disassembling the entire back end of the unit.

    imageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    there is no continuity between the base, collector, or emitter.

     

    Diode check

    It is showing .015 Volts between the collector and the yellow wire (which I believe is the base in your picture, although I'm not sure if I'm looking at the front or back side)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    The data sheet for the 2N3055 NPN power transistors specifies

     

    2N3055 Equivalents

    2N6673, 2N6675, complementary pair- MJ2955

     

    Is there something special about complementary pairs vs two NTE130s?

     

    Thanks,

    Matt

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    Discovery, by following the wires I figured out there are actually a total of (4) 2N3055 power transistors (not 2) hidden in all the heat sinks.... the blue and yellow wires are soldered to the transistor leads so removing them completely will be a chore. 

     

    Here a pic of the transistor tucked away behind a set of heat sinks...  the picture is actually upside down so I could read the description.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    I believe that the transistors are not soldered in but rather plugged into sockets. Once you have taken the screws out I believe that the transistors will unplug. At least I hope this is the case. If the wires are indeed soldered to the pins then you will have no choice except to unsolder them. The reason that they use matched pairs is so the transistors, which all vary slightly from one another, work together and share the load equally. If the transistors are badly mismatched the burden of the work will fall on the weaker of the two devices and it will fail more quickly. Keep in mind that unless there is a short between the Emitter and the Collector these transistors are not likely to be the cause of the problem with the power supply.  I am still trying to figure out what the next step is.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    I believe that the transistors are not soldered in but rather plugged into sockets. Once you have taken the screws out I believe that the transistors will unplug. At least I hope this is the case. If the wires are indeed soldered to the pins then you will have no choice except to unsolder them. The reason that they use matched pairs is so the transistors, which all vary slightly from one another, work together and share the load equally. If the transistors are badly mismatched the burden of the work will fall on the weaker of the two devices and it will fail more quickly. Keep in mind that unless there is a short between the Emitter and the Collector these transistors are not likely to be the cause of the problem with the power supply.  I am still trying to figure out what the next step is.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer