Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14782 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    Don't worry, make sure you have a clean, well-lit workspace, there is nothing proprietary or expensive about any of the parts here.  Those look, from here, to be to-218  packages, which have been supplanted by to-220, not to worry.

     

    The transistors are in sockets.  If you remove the screws (being careful to recover all of the washers) the sockets will hang on their wires, and the transistors can be pulled out.  There might be an insulating mica sheet to be careful of.  On the off chance that the transistors are different devices, you might take a picture in order to help us keep things straight.

     

    Can you test with an ohmmeter or continuity tester to see if these two transistor are wired in parallel or not?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    Don't worry, make sure you have a clean, well-lit workspace, there is nothing proprietary or expensive about any of the parts here.  Those look, from here, to be to-218  packages, which have been supplanted by to-220, not to worry.

     

    The transistors are in sockets.  If you remove the screws (being careful to recover all of the washers) the sockets will hang on their wires, and the transistors can be pulled out.  There might be an insulating mica sheet to be careful of.  On the off chance that the transistors are different devices, you might take a picture in order to help us keep things straight.

     

    Can you test with an ohmmeter or continuity tester to see if these two transistor are wired in parallel or not?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • gpsmikey
    0 gpsmikey over 11 years ago in reply to D_Hersey

    One thing to check - second image down, one lead of the diode is against the filter cap and looks like it caused the insulation on the cap to melt when it was soldered.  If that lead is NOT ground and is against the cap, it may have shorted to the shell of the cap (which is most likely ground).  Make sure there is not a short there.

     

    mikey