Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14626 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    Then again, I have a theory:  I have two existential fuzzy fax at hand.  From the WWW.  1)  The schematic is unpublished.  2)  There are a lot of dysfunctional versions of this unit on the market.

     

    Here's my guess:  The other transistor on the case is identical and wired in parallel.

     

    1 is probably because our hero may be a little chagrined.  2 Indicates design flaw.

     

    My guess is that our hero took a flyer for market reasons.

     

    Hogging over time may have forced one of your Qs to fail open.  This would account for your over-current light.

     

    My consequent guess is that a pair (possibly re-biased, maybe not) of power mosfets or lm395s instead of the 3055s or whatevs that were in there would tighten this boat up nicely. 

     

    ==========

     

    Or, all of this could be wrong.  Those with alternate theories that are parsimonious and fit the facts as we know them currently are free to come forward.

     

    The ball is in your court, Bucko.  Time for some empiricism!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    Then again, I have a theory:  I have two existential fuzzy fax at hand.  From the WWW.  1)  The schematic is unpublished.  2)  There are a lot of dysfunctional versions of this unit on the market.

     

    Here's my guess:  The other transistor on the case is identical and wired in parallel.

     

    1 is probably because our hero may be a little chagrined.  2 Indicates design flaw.

     

    My guess is that our hero took a flyer for market reasons.

     

    Hogging over time may have forced one of your Qs to fail open.  This would account for your over-current light.

     

    My consequent guess is that a pair (possibly re-biased, maybe not) of power mosfets or lm395s instead of the 3055s or whatevs that were in there would tighten this boat up nicely. 

     

    ==========

     

    Or, all of this could be wrong.  Those with alternate theories that are parsimonious and fit the facts as we know them currently are free to come forward.

     

    The ball is in your court, Bucko.  Time for some empiricism!