Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14626 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    This is a very straight forward NPN power-transistor.  http://www.onsemi.com/pub_link/Collateral/2N3055-D.PDF

    There is the mica washer as I predicted.  The manufacturer didn't overuse heat-sink compound, which is rare.  You should only use enough to fill voids in the metal, otherwise metal-metal contact is better.

     

    If you have a diode test mode on your multimeter, you should see a diode between base and emmiter.  You should see another one with a slightly lower drop collector-to-base.  The case is collector.  High Z in every other two-terminal modality.

     

    These transistors were quite rugged but had low gain.  This is a very good choice for a pass transistor.  I suspect that the power Q by the op-amps is a predriver for this, probably in Darlington configuration.  I've made a fetlington with one years ago, robust as an anchor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    This is a very straight forward NPN power-transistor.  http://www.onsemi.com/pub_link/Collateral/2N3055-D.PDF

    There is the mica washer as I predicted.  The manufacturer didn't overuse heat-sink compound, which is rare.  You should only use enough to fill voids in the metal, otherwise metal-metal contact is better.

     

    If you have a diode test mode on your multimeter, you should see a diode between base and emmiter.  You should see another one with a slightly lower drop collector-to-base.  The case is collector.  High Z in every other two-terminal modality.

     

    These transistors were quite rugged but had low gain.  This is a very good choice for a pass transistor.  I suspect that the power Q by the op-amps is a predriver for this, probably in Darlington configuration.  I've made a fetlington with one years ago, robust as an anchor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer