Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14626 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    This is your circuit in concept:

    image

    Also, proof that I have been hitting the coffee pot to excess.

     

    The amp is differential, the bubble implies inversion.  Let's say that I have the reference at one volt.  What should happen is that this should cause an output of one volt.  Let's say I increase the reference potential to 1.05V.  The amp would be imbalanced.  The output would go up in value.  This would turn Q1 on further (presuming it isn't saturated, et c.) raising the output potential while increasing the potential at the inverting input of the error amp since they are attached.  When the inverting terminal rises the delta, .05V, things settle out again, ignoring offset potential.

     

    If the output transistor is good, we can check the reference.  If it is good, we are left to conclude, in the context of proper connection, that the op-amp is having a sick day.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    This is your circuit in concept:

    image

    Also, proof that I have been hitting the coffee pot to excess.

     

    The amp is differential, the bubble implies inversion.  Let's say that I have the reference at one volt.  What should happen is that this should cause an output of one volt.  Let's say I increase the reference potential to 1.05V.  The amp would be imbalanced.  The output would go up in value.  This would turn Q1 on further (presuming it isn't saturated, et c.) raising the output potential while increasing the potential at the inverting input of the error amp since they are attached.  When the inverting terminal rises the delta, .05V, things settle out again, ignoring offset potential.

     

    If the output transistor is good, we can check the reference.  If it is good, we are left to conclude, in the context of proper connection, that the op-amp is having a sick day.