Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14633 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Continuing my observations: This is a voltage regulated power supply and the only current regulation appears to be the overload trip when the current exceeds specifications. We know the front end of the supply is working as we are getting power for the overload light. If the output transistors were shorted we would get full output voltage with no regulation. Since we have no output voltage and an indication of an over current situation the first place to look seems to be where and which components are capable of giving us a high current situation at the output when no load is attached. The test that I mentioned in my previous post should allow us to test for a full or partial short. If that is the situation it will be necessary to go through the components that are across the output and isolate and test until the culprit is found. The other possibility, though less likely, is that the overload sensor circuit itself has failed and is reading a false overload and shutting down the output for no reason.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    Continuing my observations: This is a voltage regulated power supply and the only current regulation appears to be the overload trip when the current exceeds specifications. We know the front end of the supply is working as we are getting power for the overload light. If the output transistors were shorted we would get full output voltage with no regulation. Since we have no output voltage and an indication of an over current situation the first place to look seems to be where and which components are capable of giving us a high current situation at the output when no load is attached. The test that I mentioned in my previous post should allow us to test for a full or partial short. If that is the situation it will be necessary to go through the components that are across the output and isolate and test until the culprit is found. The other possibility, though less likely, is that the overload sensor circuit itself has failed and is reading a false overload and shutting down the output for no reason.

    John