Power & Energy
  • Technologies
  • More
Power & Energy
Forum help? voltage drop 16-12v to 4v
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 286 subscribers
  • Views 4334 views
  • Users 0 members are here
  • voltage_drop
  • circuit
  • led
  • voltage
Related

help? voltage drop 16-12v to 4v

e14 Contributor
e14 Contributor over 11 years ago

Help appreciated! Is the attached voltage drop diagram correct?  I need to convert a 16-12v battery for use with a 4v LED lamp. I've bought an led desk-lamp which was sold with a DC supply rated as follows:

4v  0.75A   3W.

 

I want to use it with a 16v battery (fully charged) whose voltage drops eg down to 12v over a few hours.  IE, do I need to buy 1x16 ohm and 1 x 5.33 ohm resistor?

 

Thanks so much!

 

 

image

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi John,

    If you get one of these you can convert the 12 volts to the 4 volts without wasting as much energy as the use of resistors would entail. This is basically what Don recommended but marketed as a finished product. You should also put a current limiting resistor in series with your LEDs. Using your numbers a 5 ohm resistor would limit your current to less than .75 A at 4 volts. Once you power the converter you will need to adjust the potentiometer so that the output is the 4 volts you require before hooking up the LEDs.

     

    http://www.ebay.com/itm/7-32V-to-0-8-28V-DC-DC-Boost-Buck-Converter-12A-Constant-Current-Volt-Regulator-/301484905256?pt=LH_DefaultDomain_2&hash=item4631e69328

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    Thank so much John!  Would one of these do the job as well?

    LM2596 DC-DC Switching Adjustable Step Down Voltage Regulator Buck Converter | eBay

    It's max 2amp, which for my LED should be plenty?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    Thank so much John!  Would one of these do the job as well?

    LM2596 DC-DC Switching Adjustable Step Down Voltage Regulator Buck Converter | eBay

    It's max 2amp, which for my LED should be plenty?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi John,

    Yes this is the same animal just a slightly different chip and a little lighter duty but it should work for you.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    Thanks for your help John!