Power & Energy
  • Technologies
  • More
Power & Energy
Forum help? voltage drop 16-12v to 4v
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 286 subscribers
  • Views 4286 views
  • Users 0 members are here
  • voltage_drop
  • circuit
  • led
  • voltage
Related

help? voltage drop 16-12v to 4v

e14 Contributor
e14 Contributor over 11 years ago

Help appreciated! Is the attached voltage drop diagram correct?  I need to convert a 16-12v battery for use with a 4v LED lamp. I've bought an led desk-lamp which was sold with a DC supply rated as follows:

4v  0.75A   3W.

 

I want to use it with a 16v battery (fully charged) whose voltage drops eg down to 12v over a few hours.  IE, do I need to buy 1x16 ohm and 1 x 5.33 ohm resistor?

 

Thanks so much!

 

 

image

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    There are two approaches to take.

     

    If you use a resistive ballast the calculation goes like this:

    P=IV

    3 = 4*I

    correct, 750 mA.

     

    The drop across the ballast would be 16V - 4V (supply - LED drop) 12V

     

    V=I*R

    12=0.75 * R

    R = 12 * 4/3 = 16

     

    P=I*I*R

    =9W

    get about a 16 ohm resistor rated for about 20 W.  You put the led and ballast in series, than lay the string across the supply.  Your schematic is wrong.

     

    Also, this soln has a drawback.  Light consumes 4W, ballast 9W.  Efficiency is poor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    There are two approaches to take.

     

    If you use a resistive ballast the calculation goes like this:

    P=IV

    3 = 4*I

    correct, 750 mA.

     

    The drop across the ballast would be 16V - 4V (supply - LED drop) 12V

     

    V=I*R

    12=0.75 * R

    R = 12 * 4/3 = 16

     

    P=I*I*R

    =9W

    get about a 16 ohm resistor rated for about 20 W.  You put the led and ballast in series, than lay the string across the supply.  Your schematic is wrong.

     

    Also, this soln has a drawback.  Light consumes 4W, ballast 9W.  Efficiency is poor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • D_Hersey
    0 D_Hersey over 11 years ago in reply to D_Hersey

    Else, go with something like this.  You could enjoy at least 90 efficiency, electrically speaking.

     

    http://www.linear.com/product/LT3517

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to D_Hersey

    Thank you Don!  Looks like I'm going for a voltage regulator board off Ebay, see my follow-up question to John Wiltrout, above.