Power & Energy
  • Technologies
  • More
Power & Energy
Forum help? voltage drop 16-12v to 4v
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 286 subscribers
  • Views 4284 views
  • Users 0 members are here
  • voltage_drop
  • circuit
  • led
  • voltage
Related

help? voltage drop 16-12v to 4v

e14 Contributor
e14 Contributor over 11 years ago

Help appreciated! Is the attached voltage drop diagram correct?  I need to convert a 16-12v battery for use with a 4v LED lamp. I've bought an led desk-lamp which was sold with a DC supply rated as follows:

4v  0.75A   3W.

 

I want to use it with a 16v battery (fully charged) whose voltage drops eg down to 12v over a few hours.  IE, do I need to buy 1x16 ohm and 1 x 5.33 ohm resistor?

 

Thanks so much!

 

 

image

  • Sign in to reply
  • Cancel
Parents
  • michaelwylie
    0 michaelwylie over 11 years ago

    Typically you would drive the LED with a circuit like so:

    image

    where you set the voltage across the diode to 4 Volts, and set the current in the circuit to 750 mA. If you perform the calculations, the resistor will be 16 ohms. The issue here, as Don stated, is that a large portion of your power will be consumed by the 16 ohm resistor (P = I^2 * R = 9 W). If you are fine with that, then you're done. If you want the battery to last longer you'll require a different solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelwylie
    0 michaelwylie over 11 years ago

    Typically you would drive the LED with a circuit like so:

    image

    where you set the voltage across the diode to 4 Volts, and set the current in the circuit to 750 mA. If you perform the calculations, the resistor will be 16 ohms. The issue here, as Don stated, is that a large portion of your power will be consumed by the 16 ohm resistor (P = I^2 * R = 9 W). If you are fine with that, then you're done. If you want the battery to last longer you'll require a different solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer