Power & Energy
  • Technologies
  • More
Power & Energy
Forum help? voltage drop 16-12v to 4v
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 286 subscribers
  • Views 4330 views
  • Users 0 members are here
  • voltage_drop
  • circuit
  • led
  • voltage
Related

help? voltage drop 16-12v to 4v

e14 Contributor
e14 Contributor over 11 years ago

Help appreciated! Is the attached voltage drop diagram correct?  I need to convert a 16-12v battery for use with a 4v LED lamp. I've bought an led desk-lamp which was sold with a DC supply rated as follows:

4v  0.75A   3W.

 

I want to use it with a 16v battery (fully charged) whose voltage drops eg down to 12v over a few hours.  IE, do I need to buy 1x16 ohm and 1 x 5.33 ohm resistor?

 

Thanks so much!

 

 

image

  • Sign in to reply
  • Cancel
Parents
  • deepankarmaithani
    0 deepankarmaithani over 11 years ago

    you can use a buck converter chips for a simple solution  they are highly efficient as compared to the resistive drop circuit moreover they can be more versatile if tomorrow u decide to have more current for your led.  I would also like to suggest you that you should go for a constant current circuit  as that would have an added advantage. I made one which had the same specs. You can have my stl files if you would like to try it. they are on my blog. CREATIV[E]NGINE: 3D PRINTERS : HOW THE TECH WORKS AND MY PERSONAL EXPERIENCE WITH 3D PRINTING.

    although i havent expalned about the constant current circuit on my blog you can follow the folllowing instructables High Power LED Driver Circuits : Constant current source tweaks: #2 and #3

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to deepankarmaithani

    Thank you Dipankar!

     

    Valuable advice!

    Regards

    John

     

    On Tuesday, February 17, 2015, deepankarmaithani <messages@element14.com>

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to deepankarmaithani

    Thank you Dipankar!

     

    Valuable advice!

    Regards

    John

     

    On Tuesday, February 17, 2015, deepankarmaithani <messages@element14.com>