Power & Energy
  • Technologies
  • More
Power & Energy
Forum Can I make a parallel USB circuit to power a device from my PC?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 3300 views
  • Users 0 members are here
  • mobile
  • power
Related

Can I make a parallel USB circuit to power a device from my PC?

e14 Contributor
e14 Contributor over 11 years ago

Hey so I'm making a Virtual reality head mounted display and the LCD driver board says it needs 2A. I bought the right power source but the problem is it has to be plugged into a wall. For convenience I'd like to be able to plug the HMD into my PC when I use it because it will already be plugged in there for a video signal. While picking things up from radio shack today I saw they had both USB adapters and the plug I need to power the LCD driver board which made me wonder if I could make my own power cable that plugged into my PC but I need some help and have a few questions.

 

1. Is my PC capable of supplying 2A to my display? I just built my computer and it has a nice power supply but I've heard USB ports only deliver 1A or so.  Is cheaping out on the amps a big problem? Would there be any way to create a parallel circuit that drew amps from 2 USB ports to power the display?

     This is the display I bought - http://www.amazon.com/Tontec%C2%AE-Raspberry-Display-AT070TN90-Controller/dp/B00G60FJNG/ref=sr_1_5?ie=UTF8&qid=143328730… - Mine does have a higher             resolution though.

 

2. If step one is possible what kind of wire would I need for this cable between the USB port(s)?

 

Thank you for any help!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 11 years ago in reply to e14 Contributor +2 verified
    Using multiple ports seems to be a valid way to increase current - as long as the current from each port is kept within its limit. This requires a method of ensuring the current is evenly shared between…
  • dougw
    dougw over 11 years ago +1 suggested
    USB 2 is only specified to supply 0.5 A at 5 Volts (2.5 Watts) USB 3 can supply 0.9 A. (4.5 Watts) Your device is demanding 2 A at 12 Volts (24 Watts) so USB is not close to meeting this requirement. That…
Parents
  • dougw
    0 dougw over 11 years ago

    USB 2 is only specified to supply 0.5 A at 5 Volts (2.5 Watts)

    USB 3 can supply 0.9 A. (4.5 Watts)

     

    Your device is demanding 2 A at 12 Volts (24 Watts) so USB is not close to meeting this requirement.

    That being said your device may mot actually need 2A, that is just what they recommend as a power supply capability.

    For example, the backlight on your display requires a maximum of 0.2 A and the rest of the display probably requires even less current.

    The display will likely run from much less than 12 Volts, requiring even less power, (some of these displays will run fine down to around 9 Volts) but you would need to test it with a variable power supply to determine exactly what voltage and current are actually needed.

    Even with all of these optimizations, it is unlikely the display will work well with just 2.5 Watts.

    If you do want to try your own cable, try to keep the wire at least 22 gage or heavier to minimize power loss in the wire.

    There are lots of lithium batteries available with 12 Volt output - maybe you could embed one of them behind the display panel...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to dougw

    The display is supposed to run off of 5 to 12 volts so that shouldn't be an issue but I guess I'll have to try the display on different settings to see if 0.9A is enough (I do have USB 3.0).

    What if I used two ports for more Amps though? It seems very unconventional but if it's safe I think I'll try it.

    image

    The left circuit is kind of what I'm talking about.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to dougw

    The display is supposed to run off of 5 to 12 volts so that shouldn't be an issue but I guess I'll have to try the display on different settings to see if 0.9A is enough (I do have USB 3.0).

    What if I used two ports for more Amps though? It seems very unconventional but if it's safe I think I'll try it.

    image

    The left circuit is kind of what I'm talking about.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    The problem with a battery is it needs recharging and I'll always have to have the display cable plugged in anyways so it's not really worth it. (Unless there is a cheap solution for a wireless display in which case I'd be down for sure)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago in reply to e14 Contributor

    Using multiple ports seems to be a valid way to increase current - as long as the current from each port is kept within its limit. This requires a method of ensuring the current is evenly shared between ports.

    I have a commercial CD drive that uses 2 USB ports to get enough current - so the method is used.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to dougw

    I'll give it a try! Thanks for your help, you're a gentleman and a scholar.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    Doug is one of the best here. Thanks dougw

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    Dougs suggestion is a great one.

    Keep an an eye out for the USB C standard as well. It has power capabilities of 2-3A (10-15W) in data mode and upto 100W in charging mode.