Power & Energy
  • Technologies
  • More
Power & Energy
Forum purpose of Schottky diode in the circuit
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 280 subscribers
  • Views 4624 views
  • Users 0 members are here
Related

purpose of Schottky diode in the circuit

ravi kondeti
ravi kondeti over 4 years ago

Hello 

i came across a circuit as shown below. here 20 volt battery is used as source. microcontroller is used to switch the NMOS. i am not able to understand the use of the diode placed across the gate and source of the PMOS. can anyone explain?

Thank you 

image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 4 years ago +3 verified
    Hello, (Replying from mobile so will be brief) I think this circuit is a mess, better to look for a more appropriate one, it has quite a few flaws. Anyway it is more likely a Zener diode even though…
  • ravi kondeti
    ravi kondeti over 4 years ago in reply to shabaz +1
    hello shabaz.yes its a zener, thank you for the correction. my doubt is when supply voltage is a battery, assuming NMOS is on, even though battery is increased from 20 to 60 volts. voltage across gate…
  • dougw
    dougw over 4 years ago in reply to ravi kondeti +1 verified
    If the voltage divider is calculated to handle both high and low battery voltage extremes and circuit switching speed requirements, then the zener is just for insurance. The battery won't have transients…
Parents
  • Titi
    0 Titi over 4 years ago
    I think the diode is used so as not to exceed the 16v voltage at the gate of the pmos transistor
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kkazem
    0 kkazem over 4 years ago in reply to Titi

    Titi. You are absolutely right. Without looking at the PMOS datasheet (no P/N is given), most similar FETs have a Vgs max of 20 V. Personally, I would've used an 18V zener, but 16V is fine for this application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kkazem
    0 kkazem over 4 years ago in reply to Titi

    Titi. You are absolutely right. Without looking at the PMOS datasheet (no P/N is given), most similar FETs have a Vgs max of 20 V. Personally, I would've used an 18V zener, but 16V is fine for this application.