Power & Energy
  • Technologies
  • More
Power & Energy
Forum Single Phase to three signal generator.
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Subscribers 280 subscribers
  • Views 4451 views
  • Users 0 members are here
  • power supply
  • circuit
  • power_supply
  • power
  • power.power
Related

Single Phase to three signal generator.

Jere9522
Jere9522 over 4 years ago

Hello everyone,
I am designing a low voltage power supply that will run single phase to three phase circuit and will be using ultrosonic frequency as its signal input. The current circuit design uses three operational amplifiers that has a 60 degress phase shift. I am encountering a problem with regards to the output amplitude of the three phase signals. It seems to have a decrease in the amplitude. I also used RC oscillator circuit in front of the op-amp to have a precise phase shift. I am asking for any suggestions or how to deal with this problem? Also, are there any concept that I can study to approach this problem? I am also thinking to apply DSP filtering to elimate the noise in the output. Thank you in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 4 years ago +2 verified
    I'm not entirely sure what you're looking for, especially the ultrasonic bit! A diagram would definitely help. For the 3-phase generation portion, in theory that's quite easy using any microcontroller…
  • genebren
    genebren over 4 years ago +2 verified
    It would appear from your schematic, that because the output of the first stage, feeds the input of the second stage, and the output of the second stage feeds the input for the third, the amplitude changes…
  • jc2048
    jc2048 over 4 years ago in reply to Jere9522 +2
    Don't try it as you've drawn it. The maximum supply for a MCP6291 is 6V, 10V will blow it up.
Parents
  • shabaz
    +1 shabaz over 4 years ago

    I'm not entirely sure what you're looking for, especially the ultrasonic bit!

    A diagram would definitely help.

    For the 3-phase generation portion, in theory that's quite easy using any microcontroller with PWM, and a simple filter to construct the waveforms from that:

    /technologies/power-management/b/blog/posts/building-a-three-phase-mains-power-system-simulator

    However you may have different requirements so it needs more info. (the microcontroller approach just mentioned only works at low frequencies, not ultrasonic).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • shabaz
    +1 shabaz over 4 years ago

    I'm not entirely sure what you're looking for, especially the ultrasonic bit!

    A diagram would definitely help.

    For the 3-phase generation portion, in theory that's quite easy using any microcontroller with PWM, and a simple filter to construct the waveforms from that:

    /technologies/power-management/b/blog/posts/building-a-three-phase-mains-power-system-simulator

    However you may have different requirements so it needs more info. (the microcontroller approach just mentioned only works at low frequencies, not ultrasonic).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Jere9522
    0 Jere9522 over 4 years ago in reply to shabaz

    image

    image

    Here is my initial circuit, the output signal will be use as a frequency output for a transducer