Power & Energy
  • Technologies
  • More
Power & Energy
Forum Oscillating signal splitter into 3 output
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 280 subscribers
  • Views 2326 views
  • Users 0 members are here
Related

Oscillating signal splitter into 3 output

Jere9522
Jere9522 over 3 years ago

Hello everyone,

I am a creating a driver circuit for PZT atomizer transducer with a resonance frequency of 110kHz. The current design to split the signal in to three is by means of 3 cascaded op-amp. Also I am thinking to apply Phase locked loop in every output for the transducer to work at its resonance in the long run. 
Are there other ways to split oscillated signal into three? What techniques and concept can I apply with this? Thank you in advance for the answers, much appreciated.

This is the Oscillator circuit with cascaded amplifier as three signal splitter

image

Here is the output waveform, with 60 phase shift each output.

image

Here is the block diagram, which will be the overall system of the driver circuit.

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago +2
    If the atomizers don't all have exactly the same resonant frequency, it doesn't seem possible to lock on the resonant frequencies and still maintain a 60 degree phase shift. Why do you need to have a…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to shabaz +2
    I was thinking about this design, self oscillating at a frequency of choice (110 kHz) with the 60° 120° and 180° available: Ignore the R and C values - I just entered them to get LTSpice running…
Parents
  • dougw
    0 dougw over 3 years ago

    If the atomizers don't all have exactly the same resonant frequency, it doesn't seem possible to lock on the resonant frequencies and still maintain a 60 degree phase shift.

    Why do you need to have a fixed phase difference?

    I think it might be possible to design the phase lock circuits to have 60 degree differences without the splitter, but they couldn't lock to different resonant frequencies at the same time. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 3 years ago

    If the atomizers don't all have exactly the same resonant frequency, it doesn't seem possible to lock on the resonant frequencies and still maintain a 60 degree phase shift.

    Why do you need to have a fixed phase difference?

    I think it might be possible to design the phase lock circuits to have 60 degree differences without the splitter, but they couldn't lock to different resonant frequencies at the same time.