Power & Energy
  • Technologies
  • More
Power & Energy
Forum Giga-Ohm Resistors
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 280 subscribers
  • Views 6125 views
  • Users 0 members are here
  • giga-ohm
Related

Giga-Ohm Resistors

shabaz
shabaz over 3 years ago

Giga-ohm resistors are not all that common! : ) Especially high-voltage ones. 

I owned just a single 1Gohm resistor. I think it cost me about £10, and is useful to 2.5 kV, if it's kept entirely clean I guess.

image

Such a resistance is so high, normal multimeters are unhelpful. A Megger (Insulation Tester) on the other hand will measure it fine.

A friend sent across his constructed resistors, and it was very good, so here's a photo of it:

image

There are cutouts between each of the individual surface-mount resistors, to reduce the risk of dust/dirt build-up, which would reduce the resistance and the voltage rating.

I think I may paint over with MG 422C although MG 4226 would be better, I don't have that handy.

Anyway, I thought it was a nice solution reducing the cost of such a resistor to pennies. Each of the boards has two 1 Gohm resistances (2 x 10 x 100Mohm resistors).

Now that I have these and can keep the £10 resistor as a reference, I'm wondering if a high-voltage voltmeter could be a nice project, with a moving coil meter (I have a few moving coil panel meters lying around).

Any ideas/potential applications for these resistors would be great to hear!

  • Sign in to reply
  • Cancel

Top Replies

  • robogary
    robogary over 3 years ago +3
    The flux capacitor uses them for voltage balance when it operates a 1.21 gigawatts.
  • shabaz
    shabaz over 3 years ago in reply to michaelkellett +2
    Hi Michael, Hehe I see the 50kV one. Impressive! (Image source: Google images)
  • michaelkellett
    michaelkellett over 3 years ago +1
    A long time ago, when I was involved with designing accelerometers and associated electronics, we routinely used 100M resistors. Farnell have 0603 1G resistors (150V) at 5.43 each. They have an amazing…
  • michaelkellett
    michaelkellett over 3 years ago

    A long time ago, when I was involved with designing accelerometers and associated electronics, we routinely used 100M resistors.

    Farnell have 0603 1G resistors (150V) at 5.43 each.

    They have an amazing 50kV axial 6W1G resistor, 130mm long and £31.72 each.

    (and quite a few others as well, the cheapest is a 750V axial part at £0.578)

    I haven't wanted a 1G resistor for a very long time but recently Farnell had an offer on Vishay axial 0.5W resistors between 10M and 33M, so I bought 50 of each because I occasionally use them.

    I'm glad you mentioned this - I hadn't realised that good high value resistors were stocked to this extent.

    Your composite resistors would be more trustworthy at high voltages, especially if coated.

    I have  a 40kV rated meter probe, it has path lengthening discs and is a lot more than 130mm long (more like 300) - I wonder what is inside.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 3 years ago

    A resounding yes to your High Voltage Voltmeter idea.  Slight smile 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to michaelkellett

    Hi Michael,

    Hehe I see the 50kV one. Impressive!

    image(Image source: Google images)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 3 years ago

    I have to admit, never in my career did I ever see a Gigohm resister.

    I could see one used for a very high impedance input to say an electrostatic charge meter.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago

    I don't have any ideas but I'm really interested in whatever you build.  I do have a cheap Chinese hand cranked megger that I wonder how accurate it is.  Knowing if it even gets up to the stated voltage would be a start.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago

    The flux capacitor uses them for voltage balance when it operates a 1.21 gigawatts.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to robogary

    Well, obviously. You can’t just buy plutonium at the corner drug store Iike in 1984!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to kmikemoo

    Need a Hi pot for this baby

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to baldengineer

    Certainly not. Too many cheap counterfeit plutonium beads flooding the market. Thats why you need Mr. Fusion