Power & Energy
  • Technologies
  • More
Power & Energy
Forum Giga-Ohm Resistors
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 280 subscribers
  • Views 6127 views
  • Users 0 members are here
  • giga-ohm
Related

Giga-Ohm Resistors

shabaz
shabaz over 3 years ago

Giga-ohm resistors are not all that common! : ) Especially high-voltage ones. 

I owned just a single 1Gohm resistor. I think it cost me about £10, and is useful to 2.5 kV, if it's kept entirely clean I guess.

image

Such a resistance is so high, normal multimeters are unhelpful. A Megger (Insulation Tester) on the other hand will measure it fine.

A friend sent across his constructed resistors, and it was very good, so here's a photo of it:

image

There are cutouts between each of the individual surface-mount resistors, to reduce the risk of dust/dirt build-up, which would reduce the resistance and the voltage rating.

I think I may paint over with MG 422C although MG 4226 would be better, I don't have that handy.

Anyway, I thought it was a nice solution reducing the cost of such a resistor to pennies. Each of the boards has two 1 Gohm resistances (2 x 10 x 100Mohm resistors).

Now that I have these and can keep the £10 resistor as a reference, I'm wondering if a high-voltage voltmeter could be a nice project, with a moving coil meter (I have a few moving coil panel meters lying around).

Any ideas/potential applications for these resistors would be great to hear!

  • Sign in to reply
  • Cancel

Top Replies

  • robogary
    robogary over 3 years ago +3
    The flux capacitor uses them for voltage balance when it operates a 1.21 gigawatts.
  • shabaz
    shabaz over 3 years ago in reply to michaelkellett +2
    Hi Michael, Hehe I see the 50kV one. Impressive! (Image source: Google images)
  • michaelkellett
    michaelkellett over 3 years ago +1
    A long time ago, when I was involved with designing accelerometers and associated electronics, we routinely used 100M resistors. Farnell have 0603 1G resistors (150V) at 5.43 each. They have an amazing…
Parents
  • DAB
    DAB over 3 years ago

    I have to admit, never in my career did I ever see a Gigohm resister.

    I could see one used for a very high impedance input to say an electrostatic charge meter.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 3 years ago

    I have to admit, never in my career did I ever see a Gigohm resister.

    I could see one used for a very high impedance input to say an electrostatic charge meter.