Power & Energy
  • Technologies
  • More
Power & Energy
Forum Recondition or reuse end-of-life SLA batteries from a UPS?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 282 subscribers
  • Views 7960 views
  • Users 0 members are here
  • batteries
Related

Recondition or reuse end-of-life SLA batteries from a UPS?

baldengineer
baldengineer over 3 years ago

12V Sealed Lead Acid Battery

I realize the irony of asking this question.

If a sealed lead acid (SLA) battery is at the end of its life, then it is done, right?

I have at least six 1500 VA uninterruptible power supply (UPS) units throughout my lab, studio, and house. Each UPS has two 12 volt batteries, so I have at least two batteries total. They're slowly starting to fail because the supervisor circuit has decided the batteries are at the end of their life. (Well, in fairness, they probably are!) Fortunately, drop-in replacements exist, so I can keep the UPS units running with a swap. $150 to replace all the batteries or $1200+ for new units. (Even with 2 hours of my inflated labor charge, that is a decent saving!)

Anyway.

While I'm sure they can no longer provide 10s of amps to a load, I expect they can work as a decent low-current battery backup option for one-off IoT stuff.

Is there anything I can do to recondition these batteries? Or do I just accept their current ESR and deal with it?

Or do I just take them to the recycling center and not even bother?

What would you do?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 3 years ago +3
    If you take the top panel off (it's probably glued down) you will likely see a row of rubber vent caps underneath. If they have dimples in them then the cells have probably vented and dried out. If the…
  • Gough Lui
    Gough Lui over 3 years ago +2
    My experience is that they are rarely salvageable for anything useful. If they've been sitting in a UPS, they would likely suffer either from being dried out and bubbled up internally where adding distilled…
  • baldengineer
    baldengineer over 3 years ago in reply to beacon_dave +1
    Oh yeah.Thanks for pointing this out! You might have helped me determine the next steps. It depends on how hard it is to get those lids off. I'm sure they're glued down pretty well. Maybe I'll take…
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    If you take the top panel off (it's probably glued down) you will likely see a row of rubber vent caps underneath. If they have dimples in them then the cells have probably vented and dried out. If the cells are ok, I've heard of people successfully rehydrating them.

    I took a look at a couple of mine, found that they had vented but a couple of cells had also died so game over.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to beacon_dave

    Oh yeah.Thanks for pointing this out!

    You might have helped me determine the next steps. It depends on how hard it is to get those lids off. I'm sure they're glued down pretty well.

    Maybe I'll take the approach of whatever ones I can inspect are candidates to keep.

    I'll look into what is involved with rehydrating. But I suspect the "sealed" part of "SLA" will make that a non-starter for me. Instead, maybe I can get 2 or 3 that haven't dried out yet. Then I can use them for something else until they do.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to baldengineer

    Mine had 10 dabs of glue around the edge of the cover, so it levered off without breaking.

    If you pop the rubber cap off there is about a 5mm diameter hole into the cell, so you can rehydrate with a syringe or straw.

    I'm guessing that the battery charging circuits in these UPS units aren't up to much. I've found that most of the batteries fail within the first year or so of use. Would be interesting to find out why they are so unreliable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to baldengineer

    Here is what the dabs of glue under the cover looked like on one of mine:image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 3 years ago in reply to baldengineer

    Here is what the dabs of glue under the cover looked like on one of mine:image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • baldengineer
    baldengineer over 3 years ago in reply to beacon_dave

    Thanks! That gives me some context.

    I think after I get the swaps done, I'll look to see if one has a lid that is more willing to come off. Removing the lids will be much easier once I know where the glue is located.

    I dunno. I suspect most if not all of these will end up in recycling. But I really want to try and salvage a couple.