Power & Energy
  • Technologies
  • More
Power & Energy
Forum Recondition or reuse end-of-life SLA batteries from a UPS?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 282 subscribers
  • Views 7945 views
  • Users 0 members are here
  • batteries
Related

Recondition or reuse end-of-life SLA batteries from a UPS?

baldengineer
baldengineer over 3 years ago

12V Sealed Lead Acid Battery

I realize the irony of asking this question.

If a sealed lead acid (SLA) battery is at the end of its life, then it is done, right?

I have at least six 1500 VA uninterruptible power supply (UPS) units throughout my lab, studio, and house. Each UPS has two 12 volt batteries, so I have at least two batteries total. They're slowly starting to fail because the supervisor circuit has decided the batteries are at the end of their life. (Well, in fairness, they probably are!) Fortunately, drop-in replacements exist, so I can keep the UPS units running with a swap. $150 to replace all the batteries or $1200+ for new units. (Even with 2 hours of my inflated labor charge, that is a decent saving!)

Anyway.

While I'm sure they can no longer provide 10s of amps to a load, I expect they can work as a decent low-current battery backup option for one-off IoT stuff.

Is there anything I can do to recondition these batteries? Or do I just accept their current ESR and deal with it?

Or do I just take them to the recycling center and not even bother?

What would you do?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 3 years ago +3
    If you take the top panel off (it's probably glued down) you will likely see a row of rubber vent caps underneath. If they have dimples in them then the cells have probably vented and dried out. If the…
  • Gough Lui
    Gough Lui over 3 years ago +2
    My experience is that they are rarely salvageable for anything useful. If they've been sitting in a UPS, they would likely suffer either from being dried out and bubbled up internally where adding distilled…
  • baldengineer
    baldengineer over 3 years ago in reply to beacon_dave +1
    Oh yeah.Thanks for pointing this out! You might have helped me determine the next steps. It depends on how hard it is to get those lids off. I'm sure they're glued down pretty well. Maybe I'll take…
Parents
  • OriginalCircuit
    OriginalCircuit over 3 years ago

    Hit them with a welder and bring them back to life, Project Farm did a recent video on this and showed surprisingly good results - I've done it on the past with small batteries but sounds like it should work very well for you: www.youtube.com/watch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • OriginalCircuit
    OriginalCircuit over 3 years ago

    Hit them with a welder and bring them back to life, Project Farm did a recent video on this and showed surprisingly good results - I've done it on the past with small batteries but sounds like it should work very well for you: www.youtube.com/watch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kmikemoo
    kmikemoo over 3 years ago in reply to OriginalCircuit

    OriginalCircuit I've seen the video.  I've also seen the results of starting batteries that have failed.  I'm going to promote spending $20 on an off-brand new battery.  My 6AH 12v Miady is still going strong after 2 years ($36).  I'm getting two 4.6AH 6v batteries for the exit lights for $16.  Paranoid?  Yes.  Thank you. Laughing