Power & Energy
  • Technologies
  • More
Power & Energy
Forum What is the negative 12 volt supply used for in an ATX motherboard?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 280 subscribers
  • Views 5650 views
  • Users 0 members are here
Related

What is the negative 12 volt supply used for in an ATX motherboard?

scottiebabe
scottiebabe over 2 years ago

Technology...  Never-ending compatibility problems....

Here is the 24-pin ATX connector of my new power supply

image

Two of the pins are missing.

image

Pin 20 was formally -5V and has been omitted from ATX power supplies for a very long time.

No negative 12 volt supply for me! Somehow I missed that looking at the product spec, and no one seem to mention it either.

Here is the ATX V3.0 power specification

image

https://www.cybenetics.com/attachs/52.pdf 

The negative 12V supply is optional... great!

What is the negative 12V supply used for?

I am just going off the b350 chipset motherboard schematics available here: https://github.com/YeaTheMen/am4-motherboard/tree/main/Other%20Board%20Schematics 

In many cases nothing.

In one case an RS232 line driver/receiver 

image

In another case, an amplifier/buffer for a second audio line out for the front panel

image

Something to watch out for. In the two examples above, having the -12V rail tied to ground wouldn't be catastrophic, though the op-amp and rs232 would not function as intended... 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 2 years ago +5
    This is a known issue for a very small minority of users - generally speaking, you don't cross ATX major version numbers if you want to be sure. That means old 20-pin boards generally require an ATX 1…
  • bradfordmiller
    bradfordmiller over 2 years ago +4
    Once upon a time, EEPROMs like the 6834 would need +5 and -12; EPROMs would use +5, -5 and +12.
  • anniel747
    anniel747 over 2 years ago +1
    Deleted
Parents
  • anniel747
    anniel747 over 2 years ago
    This reply was deleted.
    • Cancel
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to anniel747

    I just referenced them, because they are easily accessible. My PC is nothing fancy a Ryzen 5 3600 with a b450 chipset...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 2 years ago in reply to anniel747

    I just referenced them, because they are easily accessible. My PC is nothing fancy a Ryzen 5 3600 with a b450 chipset...