Products
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
Power & Energy
  • Technologies
  • More
Power & Energy
Forum negative 48Vdc system to positive 48Vdc
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 279 subscribers
  • Views 1803 views
  • Users 0 members are here
Related

negative 48Vdc system to positive 48Vdc

Lemuel7
Lemuel7 over 2 years ago

Hi, I have a situation where the existing 48Vdc system is a positive grounded (-48 or negative hotwire), now I need to replace it with a new 48Vdc charger that is earth ground isolated and its output is already negative volts (positive to ground=0V & negative to ground=0V and positive to negative potential is negative 53V)

At the DC combiner panel, positive busbar was grounded and that is where we will connect in order to parallel the new system to avoid loss of dc when removing the old system.

I understand that both system outputs have different polarity hence I cannot just simply parallel them (positive grounded system does not cause polarity to change) . How do I safely remove the old system without interrupting the loads and not to loss the 48Vdc?

image

  • Sign in to reply
  • Cancel
Parents
  • Lemuel7
    0 Lemuel7 over 2 years ago

    Hi dougw

    We actually solve the issue, the 48Vdc charger was galvanically isolated so the system didn't have a common ground conductor.

    we simply connected the positive output to the ground then everything was okay, funny though sometimes the simple issues gets us confused.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Lemuel7
    0 Lemuel7 over 2 years ago

    Hi dougw

    We actually solve the issue, the 48Vdc charger was galvanically isolated so the system didn't have a common ground conductor.

    we simply connected the positive output to the ground then everything was okay, funny though sometimes the simple issues gets us confused.