Power & Energy
  • Technologies
  • More
Power & Energy
Forum DC-AC power amplification
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 279 subscribers
  • Views 1382 views
  • Users 0 members are here
Related

DC-AC power amplification

Maxbiggair
Maxbiggair over 2 years ago

 There is a kind of converter I need help on. It is a buck-boost converter but the inductor is replaced by a steel toroid core transformer with a core power of 2025W max, it has a primary input and two secondary output 250 turns 1:1:1 each. 

The transistor is changed to a MOSFET and is driven by a 555 timer pwm circuit. Powered by a 12V, 75AH Battery 

Flyback voltage is tapped out from the primary coil and the high current is tapped from the first secondary coil through the use of diode and capacitors. 

The high voltage and high current is combined and fed to the inverter converting it to 50Hz AC. The output of the inverter is connected to the first secondary coil. Which is the same coil that the high current capacitor is drawing current from.

The second secondary coil will be the output whereby a band pass filter will be used to extract the 50Hz frequency from the transformer.

The goal is to provide good efficiency while reducing the cost.

  • Sign in to reply
  • Cancel
Parents
  • kmikemoo
    kmikemoo over 2 years ago

    DUPLICATE POST.

     RE: Power amplifier using flyback converter 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Maxbiggair
    Maxbiggair over 2 years ago in reply to kmikemoo

    Kinda found out that I posted it on the wrong side

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to Maxbiggair

    Maxbiggair If you want it moved, reach out to Feedback & Support in the Members tab.  They can move it to the right place.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kmikemoo
    kmikemoo over 2 years ago in reply to Maxbiggair

    Maxbiggair If you want it moved, reach out to Feedback & Support in the Members tab.  They can move it to the right place.