Power & Energy
  • Technologies
  • More
Power & Energy
Forum Can someone provide me with teardown of chassis mount resistor tjt300 10R from TE
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 280 subscribers
  • Views 1485 views
  • Users 0 members are here
  • resistor
Related

Can someone provide me with teardown of chassis mount resistor tjt300 10R from TE

manojroy123
manojroy123 over 2 years ago

Can someone provide me with teardown of chassis mount resistor tjt300 10R from TE. What kind of strip is used inside it.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 2 years ago +3
    I think this may be a case where you need to spend £50 and do your own tearing. (Watch out for toxic stuff inside !!) Why do you want to know ? MK
  • gordonmx
    gordonmx over 2 years ago +1
    The datasheet for the resistor says wire wound. Most likely nichrome. The 300 W rating is with a heatsink and is 150 W in free air. That would lead to 3.9 amps (R*I^2) for 150W. With a 2.75" x 8" body…
Parents
  • gordonmx
    gordonmx over 2 years ago

    The datasheet for the resistor says wire wound.  Most likely nichrome.  The 300 W rating is with a heatsink and is 150 W in free air.  That would lead to 3.9 amps (R*I^2) for 150W.  With a 2.75" x 8" body, that can be a number of turns.   

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gordonmx
    gordonmx over 2 years ago

    The datasheet for the resistor says wire wound.  Most likely nichrome.  The 300 W rating is with a heatsink and is 150 W in free air.  That would lead to 3.9 amps (R*I^2) for 150W.  With a 2.75" x 8" body, that can be a number of turns.