Power & Energy
  • Technologies
  • More
Power & Energy
Forum Gate protesction against undisired switch on
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 282 subscribers
  • Views 1951 views
  • Users 0 members are here
  • gate driver
  • protection
  • marx
Related

Gate protesction against undisired switch on

finoconv
finoconv over 1 year ago

I'm designing a Marx generator with solid state switch. I'm using IGBTs.

Each IGBT has a 160uF capacitive load. At the moment I'm testing a generator that is powered with a 1kV and has 3 stages: the output voltage should be 3000V for a resistive load of 100Ohms.

Every stage of the marx is constituted by a half bridge with the gate isolated. Firstly I tested the same project with 6uF per stage and the system worked. When I try to discharge the Marx generator (with 160uF per cell) at the maximum voltage, I made the huge error to not connect any load. I heard a big burst and I noted that in one stage, the tracks of the half bridge were burned and the IGBT were faulted.

Apart from the huge mistake of not connecting the load, I'm thinking to protect the gate oh the high IGBT form the undesired switching on, due to floting voltage between the two IGBT. I saw in a marx generator (I am copying it in full) that there are a series of zener voltage and schottky diode between the gate and the emitter. Chat GPT says me that this should be a possible solution to avoid undesired switch on and protect the gate from overvoltage. It's not very clear for me how this could work.

Has anyone use it before? Any suggestion about the protection against undesired switching on for both IGBTs?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 1 year ago +1
    How about posting a circuit and some pictures of your set up. MK
Parents
  • michaelkellett
    michaelkellett over 1 year ago

    How about posting a circuit and some pictures of your set up.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 1 year ago

    How about posting a circuit and some pictures of your set up.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • finoconv
    finoconv over 1 year ago in reply to michaelkellett

    Hi Michael, here is the final IGBT

    image

    And here is each gate driver stage

    image

    Here the layout and highlighted the burned tracks (they correspond to collector high, emitterhigh/collector low and emitter low)

    image

    Any suggestion will be precious.

    Thanks