Power & Energy
  • Technologies
  • More
Power & Energy
Forum What is you surge suppression experience
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 281 subscribers
  • Views 1242 views
  • Users 0 members are here
  • surge_suppression
  • lightning
  • protection
Related

What is you surge suppression experience

colporteur
colporteur 2 months ago

image

Key Features • Supports 10/100/1000/10GBASE-T Ethernet speeds • Full PoE, PoE+, and PoE++ (IEEE 802.3af/at/bt) compatibility • Supports up to 90W of power delivery • IP65-rated waterproof outdoor enclosure • Designed to protect against lightning strikes and electrical surges • Ultra-low capacitance for high-speed data performance • Fast response time for critical equipment protection • Simple inline RJ45 installation • Flexible mounting options for poles, enclosures, and walls • Tested to international surge protection standards Ideal Applications • Outdoor wireless radios and backhaul links • Fixed wireless and WISP deployments • Outdoor WiFi access points • IP surveillance and security cameras • Network switches and outdoor enclosures • Industrial networking and SCADA systems • Municipal, campus, and enterprise network infrastructure

I am on my third install of CAT6 cables to Access points on the top of grain bins. This advertisement for Data Surge Protection Outdoor SPD IP65 10GB Ethernet came across my desk.

Many a fault over 20 years working in telecommunications were repaired on two wire copper pairs by replacing the fuse or surge suppressor. I never gave a thought to network cable. Then I was never running them up the side of grain bins. Now I'm thinking about them after the ad appeared to remind me.

Looking to find anyone that has experience and can provide some insight.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur 2 months ago in reply to Jan Cumps +2
    The CAT6 cable runs are outside the bin. On some other bins there are GPS antennas and cameras. I default to the yard supervisor for installation. He hasn't told me NO to this point. I would have thought…
  • kmikemoo
    kmikemoo 2 months ago in reply to colporteur +2
    Ah... so kind of telecom to provide you with some lightning protection. I think you are at low risk of a direct strike but still at average risk of the elevated ground plane created by a near lightning…
  • kmikemoo
    kmikemoo 2 months ago in reply to colporteur +2
    That is a reasonable question. Another IT guy would probably read any notes you have on the AP or network map. To everyone else... connectivity is magic. Even if you tell them, they will forget. SO...…
Parents
  • shabaz
    shabaz 2 months ago

    Hi Sean,

    I was googling and found this product which looks interesting: Citel MJ8-POE-C6A

    The datasheet has this diagram:

    image

    I've never seen three-terminal GDT's before, but the Cyclone product you found uses three-terminal ones too. However, the MJ8-POE-C6A also includes a lot more.

    This is the Cyclone circuit from their datasheet:

    image

    The Citel one has a shielded metal enclosure, plus also has silicon devices (for faster action; the GDTs will be slower) for differential-mode within each pair, but also between two pairs. Not sure why the two central pairs in that diagram don't have the same arrangement, anyone know?

    Also, I was wondering, it might be a good idea to buy ferrites too, and clip them at each end, to suppress common-mode spikes, so the diodes and GDTs have to do less work. They would have to be quite large ferrites.

    I bought these a while back:

    image

    I wasn't planning to use them for network connections, but because I wanted to fit an antenna outdoors and was worried about induced voltages during thunderstorms. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz 2 months ago in reply to shabaz

    Also, reading more, apparently another path is through the mains supply to your network equipment, because any lightning strike to earth will create a huge voltage difference in earth, and that means that the line+neutral can become temporarily at a massively different voltage to local earth or to earth near your Ethernet cable. Just a few picofarad capacitance to ground will therefore cause massive current to flow. There are DIN mount surge protectors for the mains. I don't know anything about these, but hopefully an electrician may know. So, a holistic approach may need the surge protection on both the mains entry (and check it has line/neutral to Earth protection, not just line to neutral like cheap mains extension surge protectors) as well as the surge protection at the Ethernet cable (both ends, and ideally with TVS as well as GDT) and add large ferrites at the Ethernet cable (both ends) too.

    Total speculation however.. this is well outside my comfort area : (

    Also maybe worth considering optical if possible : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz 2 months ago in reply to shabaz

    Also, reading more, apparently another path is through the mains supply to your network equipment, because any lightning strike to earth will create a huge voltage difference in earth, and that means that the line+neutral can become temporarily at a massively different voltage to local earth or to earth near your Ethernet cable. Just a few picofarad capacitance to ground will therefore cause massive current to flow. There are DIN mount surge protectors for the mains. I don't know anything about these, but hopefully an electrician may know. So, a holistic approach may need the surge protection on both the mains entry (and check it has line/neutral to Earth protection, not just line to neutral like cheap mains extension surge protectors) as well as the surge protection at the Ethernet cable (both ends, and ideally with TVS as well as GDT) and add large ferrites at the Ethernet cable (both ends) too.

    Total speculation however.. this is well outside my comfort area : (

    Also maybe worth considering optical if possible : )