Power & Energy
  • Technologies
  • More
Power & Energy
Forum What is you surge suppression experience
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 282 subscribers
  • Views 1021 views
  • Users 0 members are here
  • surge_suppression
  • lightning
  • protection
Related

What is you surge suppression experience

colporteur
colporteur 1 month ago

image

Key Features • Supports 10/100/1000/10GBASE-T Ethernet speeds • Full PoE, PoE+, and PoE++ (IEEE 802.3af/at/bt) compatibility • Supports up to 90W of power delivery • IP65-rated waterproof outdoor enclosure • Designed to protect against lightning strikes and electrical surges • Ultra-low capacitance for high-speed data performance • Fast response time for critical equipment protection • Simple inline RJ45 installation • Flexible mounting options for poles, enclosures, and walls • Tested to international surge protection standards Ideal Applications • Outdoor wireless radios and backhaul links • Fixed wireless and WISP deployments • Outdoor WiFi access points • IP surveillance and security cameras • Network switches and outdoor enclosures • Industrial networking and SCADA systems • Municipal, campus, and enterprise network infrastructure

I am on my third install of CAT6 cables to Access points on the top of grain bins. This advertisement for Data Surge Protection Outdoor SPD IP65 10GB Ethernet came across my desk.

Many a fault over 20 years working in telecommunications were repaired on two wire copper pairs by replacing the fuse or surge suppressor. I never gave a thought to network cable. Then I was never running them up the side of grain bins. Now I'm thinking about them after the ad appeared to remind me.

Looking to find anyone that has experience and can provide some insight.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur 1 month ago in reply to Jan Cumps +2
    The CAT6 cable runs are outside the bin. On some other bins there are GPS antennas and cameras. I default to the yard supervisor for installation. He hasn't told me NO to this point. I would have thought…
  • kmikemoo
    kmikemoo 1 month ago in reply to colporteur +2
    Ah... so kind of telecom to provide you with some lightning protection. I think you are at low risk of a direct strike but still at average risk of the elevated ground plane created by a near lightning…
  • kmikemoo
    kmikemoo 1 month ago in reply to colporteur +2
    That is a reasonable question. Another IT guy would probably read any notes you have on the AP or network map. To everyone else... connectivity is magic. Even if you tell them, they will forget. SO...…
Parents
  • Jan Cumps
    Jan Cumps 1 month ago
    colporteur said:
    this is preventative or paranoid i haven't decided yet.

    adding to the paranoia: is it safe to have long copper wires (like ethernet) up a grain bin? They are prone to dust explosions. A lightning or surge event near a length of copper wires can generate a spark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur 1 month ago in reply to Jan Cumps

    The CAT6 cable runs are outside the bin. On some other bins there are GPS antennas and cameras. I default to the yard supervisor for installation. He hasn't told me NO to this point.

    I would have thought lighting rods would have been the norm on bins but not here. Over 90 bins some as high as 90 feet and not a lighting rod to be seen. The yard site is adjacent to a 1000ft telecommunication I figure that might be the lighting rod:) The guy wires from the tower cut through part of the yard.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image
     tower. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo 1 month ago in reply to colporteur

    Ah... so kind of telecom to provide you with some lightning protection.  I think you are at low risk of a direct strike but still at average risk of the elevated ground plane created by a near lightning strike - caused by the relative proximity to the telecon tower. and the inability of Mother Earth to dissipate that much energy instantaneously.
    Now... if it hasn't presented itself as a problem up to this point, your efforts will be "taking a reasonable protective posture".  You can make a sound financial decision.  If the isolators are just a fraction of the cost of the equipment they protect... go for it.  If they are even 25% the cost and you have never experienced an equipment failure from a near lightning event... put your money into other things.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur 1 month ago in reply to kmikemoo

    The video is taken from the new legg completed about May. Just to the left on the start of the video is the communications tower. I estimate 100m away.

    At the end of the video there is a 125 ft grain auger. The end of the auger points to four bins in a row. then a large silver bin. That is the north part of the yard. The bin farthermost from the silver bin has a point to point link back to where I am standing. That PTP is has a AP.

    Sorry for the noise. I never realize it. I am standing next to the belt motors that move grain both up/down and across to different bins.

    Biggest concern about putting them in is knowledge transfer. I would know they are there and what to look for. Since they are not common in networks would others?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo 1 month ago in reply to colporteur

    That is a reasonable question.  Another IT guy would probably read any notes you have on the AP or network map.  To everyone else... connectivity is magic.  Even if you tell them, they will forget.  SO... The label maker may seem like an old guy thing BUT... it works.  Slap an "Isolator Installed" label on the AP and PTP cable ends.  Sometimes, in the heat of the moment, even we forget stuff.  A little reminder can help a lot.

    For the isolators we installed, they were physically close enough to the equipment that their existence was reasonably obvious.  They also have a data tag.  If a technician couldn't figure out where to go from there... I didn't want them working on the equipment anyway.  Rude?  Maybe.  Back to Troubleshooting 101, right?  Is it receiving power?  Is it receiving input?  As I taught my techs... No gozinta = no gozouta.  (Goes in to / Goes out of).
    The reality is that, most of the time, they figure it out. Thumbsup - unless you keep rescuing them. Joy

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds 1 month ago in reply to colporteur
    colporteur said:
    gibt es GPS-Antennen und Kameras.

    GPS? shure? Or are they WLAN-antennas?

    All these buildings needing a potential ground system, a lightning rod from the roof to the ground.

    What's in the Silos?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds 1 month ago in reply to colporteur
    colporteur said:
    gibt es GPS-Antennen und Kameras.

    GPS? shure? Or are they WLAN-antennas?

    All these buildings needing a potential ground system, a lightning rod from the roof to the ground.

    What's in the Silos?