Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging two 18650 in series with USB.
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 284 subscribers
  • Views 2140 views
  • Users 0 members are here
Related

Charging two 18650 in series with USB.

jacobtc
jacobtc over 8 years ago

I'm pretty much trying to make a 7.4V battery pack, however it is critical that it can be charged through USB (5V).

So I have some 3000mAh LG cells, and that is pretty much it.

 

I know they need to be balanced, so something like this should do the trick: Link

 

However as that board needs 9V, I was thinking about boosting the 5V through this: Link

 

 

I hope it is easy to understand. Please tell me if I risk burning down my house, as that would be less optimal.

 

 

Regard

Jacob

  • Sign in to reply
  • Cancel

Top Replies

  • jacobtc
    jacobtc over 8 years ago in reply to the-dubster +2
    Yes, the 18650's do have protection. I probably won't be charging with more than 1A, so I hope the buck will be up to the task. I don't understand your last question. I intend to leave all hardware connected…
  • jacobtc
    jacobtc over 8 years ago in reply to the-dubster +2
    I will probably discharge the batteries directly from the battery terminals, as my diagram shows.
  • the-dubster
    the-dubster over 8 years ago +1
    The first link appears to be a 2S charge / discharge controller - so far so good. As you're creating the battery pack from 2 x LiPo batteries (at a guess) then that should be fine. As for using the buck…
  • the-dubster
    the-dubster over 8 years ago

    The first link appears to be a 2S charge / discharge controller - so far so good. As you're creating the battery pack from 2 x LiPo batteries (at a guess) then that should be fine.

     

    As for using the buck / boost convertor - that's usually ok too, I recently bought a bunch of those from eBay and they should work just fine.

     

    Regarding the specifications for the buck / boost, 2A is fairly generous I'd suggest - I'd figure about 1A output will be about right (2A for short periods but not really continuous unless rated as constant), output ripple is a bit crappy usually but for your application I'd think it should be fine.

     

    One final question, do the 18650 cells you're using have a built in protection circuit? (If they do then they're usually slightly longer than the non-protected cells).  If they do have protection then are you intending to leave the charge controller connected too during use? I honestly don't know how that will work out (possibly fine but no idea).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jacobtc
    jacobtc over 8 years ago in reply to the-dubster

    Yes, the 18650's do have protection.

     

    I probably won't be charging with more than 1A, so I hope the buck will be up to the task.

     

    I don't understand your last question. I intend to leave all hardware connected yes, and charge it through USB when necessary. I'll draw a diagram:

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • the-dubster
    the-dubster over 8 years ago in reply to jacobtc

    jacobtc I was just wondering if you would be supplying the load through the BMS as shown in the diagram within the aliexpress link.

     

    image

     

    The reason is, the BMS has cell over discharge protection but so do the cells, I don't know if the two will work together - it may be fine but I honestly don't know.

     

    If you're supplying the load directly from the batteries then the cell protection prevents over discharge and the BMS prevents over charge.

     

    Hopefully this clarifies.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jacobtc
    jacobtc over 8 years ago in reply to the-dubster

    I will probably discharge the batteries directly from the battery terminals, as my diagram shows.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • the-dubster
    the-dubster over 8 years ago in reply to jacobtc

    Then you should be good to go. BMS for overcharging protection (and of course balance) and inbuilt cell protection for over discharge by the load.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jacobtc
    jacobtc over 8 years ago in reply to the-dubster

    Sounds good!

    I will be 3D printing an enclosure for everything in the end.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • the-dubster
    the-dubster over 8 years ago in reply to jacobtc

    One final thing I've just thought about, re: the USB charging, is it from a PC USB port or a 'wall wart' type USB mains supply? The only reason I ask is because a PC USB port supplies around 500mA (and around 900mA for USB 3) so this would limit available charting current, an external (mains powered) supply opens up your current supply options considerably.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jacobtc
    jacobtc over 8 years ago in reply to the-dubster

    The charging will be from computers, wall adaptors and the like. The battery pack I'm making is for when I don't have access to an otherwise larger powersupply, which would normally charge the battery pack which came with the product.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • the-dubster
    the-dubster over 8 years ago in reply to jacobtc

    Charging will be quicker when using the wall adaptor obviously (unless it's 500mA or lower of course, be sure to post back here when it's done, it'd be nice to see how it turns out.