Power & Energy
  • Technologies
  • More
Power & Energy
Forum Automatic generator start
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 284 subscribers
  • Views 1515 views
  • Users 0 members are here
Related

Automatic generator start

andrequeiroz.com
andrequeiroz.com over 7 years ago

My electricity grid is dropping frequently. When the power drops, I have to manually connect a small diesel generator.

I would like to use a raspberry to automate the triggering of the generator.

Which sensor should I use to detect the power drop ?

 

ops: 380v

 

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +3
    It would seem that you need a battery or uninterruptible power supply to run the Raspberry Pi when the power fails. A simpler method would be to have a relay that is powered by mains voltage. When the…
  • jw0752
    jw0752 over 7 years ago +3
    Hi Andre, I like dougw suggestion and I would also look to include some sort of Hysteresis so that once the relay triggers the start of the generator and the switching of the power grid from external to…
  • a531016
    a531016 over 7 years ago +3
    Andre, The simplist verson of monitoring mains voltage is a relay with a 380V coil, and a normally closed secondary. This would open on power failure, and the RPI can start the generator (assuming an electronic…
Parents
  • jw0752
    jw0752 over 7 years ago

    Hi Andre,

    I like dougw  suggestion and I would also look to include some sort of Hysteresis so that once the relay triggers the start of the generator and the switching of the power grid from external to internal this process continues for 10 minutes or more even if the external power grid comes back on. You will need a mechanized transfer switch so that your electrical service sees only the external grid or the generator and not both. This switch should also rule out the possibility of the generator being connected to the external grid. The coil of the relay Doug recommended will be connected to the external grid even if the system is on the generator. You will have to make sure there is isolation between the internal system and this relay coil so that you do not accidentally bridge the two grids. There may be some commercial products that do these procedures for you. If you make the modifications and design yourself you are signing up for some serious liability if things go wrong. Depending on where you live in the world this may be regulated or not. In any case do it safely. I remember the recommendation of a friend who was admittedly ignorant of electricity. He used to say that he only knew two things about electricity. #1 If you don't pay the bill they turn it off. #2 If you play with it, it will kill you.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • andrequeiroz.com
    andrequeiroz.com over 7 years ago in reply to jw0752

    Hi, Mr. John, I need to send more details of the operation that is done manually today.

    I agree with your friend, electricity punishes the inattentive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • andrequeiroz.com
    andrequeiroz.com over 7 years ago in reply to jw0752

    Hi, Mr. John, I need to send more details of the operation that is done manually today.

    I agree with your friend, electricity punishes the inattentive.